TBSSmoothBuilder Class¶
-
class
NXOpen.CAE.Optimization.
TBSSmoothBuilder
¶ Bases:
NXOpen.Builder
Represents the builder of
NXOpen.CAE.Optimization.TBSSmooth
.To create a new instance of this class, use
NXOpen.CAE.Optimization.TBSOptimizationManager.CreateSmoothBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Border | Returns or sets the option to save border. |
ComponentLimitingSize | Returns the limiting size that defines the minimal allowed relative size of a connected component. |
IsoTypeOption | Returns or sets the option that specifies what should be saved to the output files |
IsoValue | Returns or sets the iso value that is used to determine the positions on the element edges where the new nodes are created. |
MinimumAngle | Returns the minimum angle that defines the minimal angle of the triangles that result from the smoothing and data reduction. |
MixedMesh | Returns or sets the choice whether to form quardrilaterals from adjacent triangles |
NameDescription | Returns the name description |
OriginalSurfaceSmooth | Returns or sets the option of how to smooth the original surface |
ReductionAngle | Returns the reduction angle that defines the maximal angle between adjacent faces at a node such that the node may be removed during the data reduction |
ReductionRate | Returns or sets the reduction rate that defines the percent of faces that should be removed during the data reduction. |
ResultFilteringOption | Returns or sets the result filtering option |
SelfIntersectionChecking | Returns or sets the option of self-intersection checking |
SliceFormat | Returns or sets the slice format |
SliceNormalVector | Returns or sets the slice normal vector |
SliceNumber | Returns or sets the slice number |
SmoothArea | Returns the area to be smoothed |
SmoothCycles | Returns or sets the number of smoothing cycles. |
Tag | Returns the Tag for this object. |
TargetVolume | Returns or sets the target volume that is to be achieved iteratively by varying the isovalue. |
UseAdditionalParameters | Returns or sets the option to use additional parameter. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFormatOption | The output result format accessor |
GetObject | Returns the object currently being edited by this builder. |
SetFormatOption | The output result format mutator |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TBSSmoothBuilderFormat Enumeration | Defines the output file format of surface representation |
TBSSmoothBuilderIsoType Enumeration | Specifies the content saved to the output files |
TBSSmoothBuilderOriginalSurfaceSmoothingOption Enumeration | Defines if the original surface is to be smoothed or remain unchanged |
TBSSmoothBuilderResultFiltering Enumeration | Defines if the element material values are to be filtered before the isocut |
TBSSmoothBuilderSelfIntersectionCheckingOption Enumeration | Defines if the self-itersection checks are to be performed during the isocut, smoothing and data reduction |
TBSSmoothBuilderSliceFormatOption Enumeration | Defines how to save slices |
Property Detail¶
Border¶
-
TBSSmoothBuilder.
Border
¶ Returns or sets the option to save border.
If yes, the border of the shell element model will saved
-------------------------------------
Getter Method
Signature
Border
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Border
Parameters: border (bool) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
ComponentLimitingSize¶
-
TBSSmoothBuilder.
ComponentLimitingSize
¶ Returns the limiting size that defines the minimal allowed relative size of a connected component.
All components with the relative size below this value are removed
-------------------------------------
Getter Method
Signature
ComponentLimitingSize
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
IsoTypeOption¶
-
TBSSmoothBuilder.
IsoTypeOption
¶ Returns or sets the option that specifies what should be saved to the output files
-------------------------------------
Getter Method
Signature
IsoTypeOption
Returns: Return type: NXOpen.CAE.Optimization.TBSSmoothBuilderIsoType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsoTypeOption
Parameters: isoTypeOption ( NXOpen.CAE.Optimization.TBSSmoothBuilderIsoType
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
IsoValue¶
-
TBSSmoothBuilder.
IsoValue
¶ Returns or sets the iso value that is used to determine the positions on the element edges where the new nodes are created.
Larger value lead to models with smaller volume. Value is between 0 and 1
-------------------------------------
Getter Method
Signature
IsoValue
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsoValue
Parameters: isoValue (float) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
MinimumAngle¶
-
TBSSmoothBuilder.
MinimumAngle
¶ Returns the minimum angle that defines the minimal angle of the triangles that result from the smoothing and data reduction.
Too large value may prevent the smoothing, and too small value may lead to degenerated triangles
-------------------------------------
Getter Method
Signature
MinimumAngle
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
MixedMesh¶
-
TBSSmoothBuilder.
MixedMesh
¶ Returns or sets the choice whether to form quardrilaterals from adjacent triangles
-------------------------------------
Getter Method
Signature
MixedMesh
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MixedMesh
Parameters: mixedMesh (bool) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
NameDescription¶
-
TBSSmoothBuilder.
NameDescription
¶ Returns the name description
-------------------------------------
Getter Method
Signature
NameDescription
Returns: Return type: NXOpen.CAE.Optimization.NameDescription
New in version NX8.0.0.
License requirements: None.
OriginalSurfaceSmooth¶
-
TBSSmoothBuilder.
OriginalSurfaceSmooth
¶ Returns or sets the option of how to smooth the original surface
-------------------------------------
Getter Method
Signature
OriginalSurfaceSmooth
Returns: Return type: NXOpen.CAE.Optimization.TBSSmoothBuilderOriginalSurfaceSmoothingOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OriginalSurfaceSmooth
Parameters: originalSurfaceSmooth ( NXOpen.CAE.Optimization.TBSSmoothBuilderOriginalSurfaceSmoothingOption
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
ReductionAngle¶
-
TBSSmoothBuilder.
ReductionAngle
¶ Returns the reduction angle that defines the maximal angle between adjacent faces at a node such that the node may be removed during the data reduction
-------------------------------------
Getter Method
Signature
ReductionAngle
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ReductionRate¶
-
TBSSmoothBuilder.
ReductionRate
¶ Returns or sets the reduction rate that defines the percent of faces that should be removed during the data reduction.
if set to 0, no data reduction occurs. If set to 100, the data reduction sopts when no faces could be removed
-------------------------------------
Getter Method
Signature
ReductionRate
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReductionRate
Parameters: reductionRate (float) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
ResultFilteringOption¶
-
TBSSmoothBuilder.
ResultFilteringOption
¶ Returns or sets the result filtering option
-------------------------------------
Getter Method
Signature
ResultFilteringOption
Returns: Return type: NXOpen.CAE.Optimization.TBSSmoothBuilderResultFiltering
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResultFilteringOption
Parameters: resultFilteringOption ( NXOpen.CAE.Optimization.TBSSmoothBuilderResultFiltering
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
SelfIntersectionChecking¶
-
TBSSmoothBuilder.
SelfIntersectionChecking
¶ Returns or sets the option of self-intersection checking
-------------------------------------
Getter Method
Signature
SelfIntersectionChecking
Returns: Return type: NXOpen.CAE.Optimization.TBSSmoothBuilderSelfIntersectionCheckingOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelfIntersectionChecking
Parameters: selfIntersectionChecking ( NXOpen.CAE.Optimization.TBSSmoothBuilderSelfIntersectionCheckingOption
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
SliceFormat¶
-
TBSSmoothBuilder.
SliceFormat
¶ Returns or sets the slice format
-------------------------------------
Getter Method
Signature
SliceFormat
Returns: Return type: NXOpen.CAE.Optimization.TBSSmoothBuilderSliceFormatOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SliceFormat
Parameters: sliceFormat ( NXOpen.CAE.Optimization.TBSSmoothBuilderSliceFormatOption
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
SliceNormalVector¶
-
TBSSmoothBuilder.
SliceNormalVector
¶ Returns or sets the slice normal vector
-------------------------------------
Getter Method
Signature
SliceNormalVector
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SliceNormalVector
Parameters: sliceNormalVector ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
SliceNumber¶
-
TBSSmoothBuilder.
SliceNumber
¶ Returns or sets the slice number
-------------------------------------
Getter Method
Signature
SliceNumber
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SliceNumber
Parameters: sliceNumber (int) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
SmoothArea¶
-
TBSSmoothBuilder.
SmoothArea
¶ Returns the area to be smoothed
-------------------------------------
Getter Method
Signature
SmoothArea
Returns: Return type: NXOpen.CAE.Optimization.TBSGroupDefinition
New in version NX8.0.0.
License requirements: None.
SmoothCycles¶
-
TBSSmoothBuilder.
SmoothCycles
¶ Returns or sets the number of smoothing cycles.
If set to 0, no smoothing is performed. Larger value leads to smoother models, but may cause the narrowing of thin components
-------------------------------------
Getter Method
Signature
SmoothCycles
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothCycles
Parameters: smoothCycles (int) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
TargetVolume¶
-
TBSSmoothBuilder.
TargetVolume
¶ Returns or sets the target volume that is to be achieved iteratively by varying the isovalue.
If set to 0, the given
NXOpen.CAE.Optimization.TBSSmoothBuilder.IsoValue`()
is usedfor the generation of the isosurface-------------------------------------
Getter Method
Signature
TargetVolume
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetVolume
Parameters: targetVolume (float) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
UseAdditionalParameters¶
-
TBSSmoothBuilder.
UseAdditionalParameters
¶ Returns or sets the option to use additional parameter.
-------------------------------------
Getter Method
Signature
UseAdditionalParameters
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseAdditionalParameters
Parameters: useAdditionalParameters (bool) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Method Detail¶
GetFormatOption¶
-
TBSSmoothBuilder.
GetFormatOption
¶ The output result format accessor
Signature
GetFormatOption()
Returns: Return type: list of NXOpen.CAE.Optimization.TBSSmoothBuilderFormat
New in version NX8.0.0.
License requirements: None.
SetFormatOption¶
-
TBSSmoothBuilder.
SetFormatOption
¶ The output result format mutator
Signature
SetFormatOption(formatOption)
Parameters: formatOption (list of NXOpen.CAE.Optimization.TBSSmoothBuilderFormat
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Validate¶
-
TBSSmoothBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.