TBSGroupDefinition Class¶
-
class
NXOpen.CAE.Optimization.
TBSGroupDefinition
¶ Bases:
NXOpen.TaggedObject
Represents a group of nodes or elements
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Definition | Returns or sets the definition type |
Tag | Returns the Tag for this object. |
TargetSet | Returns the target set |
Methods¶
Method | Description |
---|---|
GetElementType | Returns the group element type |
Enumerations¶
TBSGroupDefinitionDefinitionType Enumeration | Represents the definition method of a group |
TBSGroupDefinitionGroupElementType Enumeration | Represents the type of group elements |
Property Detail¶
Definition¶
-
TBSGroupDefinition.
Definition
¶ Returns or sets the definition type
-------------------------------------
Getter Method
Signature
Definition
Returns: Return type: NXOpen.CAE.Optimization.TBSGroupDefinitionDefinitionType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Definition
Parameters: definition ( NXOpen.CAE.Optimization.TBSGroupDefinitionDefinitionType
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
TargetSet¶
-
TBSGroupDefinition.
TargetSet
¶ Returns the target set
-------------------------------------
Getter Method
Signature
TargetSet
Returns: Return type: NXOpen.CAE.SetManager
New in version NX8.0.0.
License requirements: None.
Method Detail¶
GetElementType¶
-
TBSGroupDefinition.
GetElementType
¶ Returns the group element type
Signature
GetElementType()
Returns: Return type: NXOpen.CAE.Optimization.TBSGroupDefinitionGroupElementType
New in version NX8.0.0.
License requirements: None.