TBSGroupDefinitionDefinitionType Enumeration¶
NXOpen.CAE.Optimization.TBSGroupDefinition.DefinitionType is an alias for NXOpen.CAE.Optimization.TBSGroupDefinitionDefinitionType
-
class
NXOpen.CAE.Optimization.
TBSGroupDefinitionDefinitionType
¶ Bases:
object
Represents the definition method of a group
Enum Members
Enum Member Enum Member Description All Defines a group with all nodes or elements Selected Defines a group by selection DesignArea Defines a group refer to design area MeshSmoothingArea Defines a group refer to mesh smoothing area -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-