SetManager Class¶
-
class
NXOpen.CAE.
SetManager
¶ Bases:
NXOpen.NXObject
Represents a group of CAE object sets. The objects in each set can be used to create loads, constraints ..etc
This is a sub object
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
TargetSetCount | Returns the count of objects in the set |
Methods¶
Method | Description |
---|---|
CleanTargetSet | Clears the objects stored in the set specified in the set manager |
CreateAttributeIterator | Create an attribute iterator |
CreateCaeSet | Creates a CAE. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTargetSetDistributedPlanes | Gets the parameters for a distributed planes set. |
GetTargetSetExcludedMembers | Gets the objects for the specified target set excluded set |
GetTargetSetGroup | Gets the CAE group in the specified set |
GetTargetSetMembers | Gets the objects for the specified target set |
GetTargetSetPlane | Gets the parameters from a plane target set. |
GetTargetSetPlaneWithOffset | Gets the parameters from a plane target set. |
GetTargetSetPointLocation | Gets the position from a point location target set. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTargetSetDistributedPlanes | Sets the parameters for a distributed planes set. |
SetTargetSetEdgePath | Sets the CAE edge path in the specified set |
SetTargetSetElemEdgePath | Sets the CAE element edge path in the specified set |
SetTargetSetExcludedMembers | Sets the CAE objects in the specified target set exclude set |
SetTargetSetGroup | Sets the CAE group in the specified set |
SetTargetSetMembers | Sets the CAE objects in the specified set |
SetTargetSetPlane | Creates a plane target set. |
SetTargetSetPlaneWithOffset | Creates a plane target set. |
SetTargetSetPointLocation | Creates a point location target set. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
SetManagerDistributedPlanesBboxType Enumeration | Used to specify which bounding box defines the position or radius of the sphere |
SetManagerDistributedPlanesBoundingSphereDirection Enumeration | Used to specify the method to define the Z+ direction of the sphere |
SetManagerDistributedPlanesBoundingSphereType Enumeration | Used to specify the type of bounding sphere to lay the distributed planes on |
SetManagerDistributedPlanesPosition Enumeration | Used to specify the method to define the position or the radius of the sphere |
Property Detail¶
IsOccurrence¶
-
SetManager.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SetManager.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SetManager.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SetManager.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SetManager.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SetManager.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
TargetSetCount¶
-
SetManager.
TargetSetCount
¶ Returns the count of objects in the set
-------------------------------------
Getter Method
Signature
TargetSetCount
Returns: count of number of sets possible in this set manager Return type: int New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
CleanTargetSet¶
-
SetManager.
CleanTargetSet
¶ Clears the objects stored in the set specified in the set manager
Signature
CleanTargetSet(setIndex)
Parameters: setIndex (int) – index of the set in the set manager New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateCaeSet¶
-
SetManager.
CreateCaeSet
¶ Creates a CAE.
CAESet
Signature
CreateCaeSet()
Returns: the cae set created Return type: NXOpen.CAE.CAESet
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
SetManager.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetTargetSetDistributedPlanes¶
-
SetManager.
GetTargetSetDistributedPlanes
¶ Gets the parameters for a distributed planes set.
Signature
GetTargetSetDistributedPlanes(setIndex)
Parameters: setIndex (int) – Index of the set Returns: a tuple Return type: A tuple consisting of (centerMethod, centerPoint, radiusMethod, radiusFactor, radiusValue, bboxOption, bboxElems, spaceDefinition, sphereDirection, sphereDirectionVector, sphereDirectionPoint1, sphereDirectionPoint2, sphereDirectionPoint3, flipNormal, refinementLevel). centerMethod is a NXOpen.CAE.SetManagerDistributedPlanesPosition
. Method used to define the sphere center centerPoint is aNXOpen.Point
. Sphere manual center position. radiusMethod is aNXOpen.CAE.SetManagerDistributedPlanesPosition
. Method used to define the sphere radius radiusFactor is aNXOpen.Expression
. Multiplying factor applied to the model bounding box diagonal to get the sphere radius. radiusValue is aNXOpen.Expression
. Radius mahual value. bboxOption is aNXOpen.CAE.SetManagerDistributedPlanesBboxType
. Bounding box definition option bboxElems is a list ofNXOpen.CAE.FEElement
. Selection used to calculate the bounding box for the manual bounding box option spaceDefinition is aNXOpen.CAE.SetManagerDistributedPlanesBoundingSphereType
. Type of bounding sphere (half or full) sphereDirection is aNXOpen.CAE.SetManagerDistributedPlanesBoundingSphereDirection
. Sphere direction definition method sphereDirectionVector is aNXOpen.Direction
. For the sphere vector method: sphere direction vector sphereDirectionPoint1 is aNXOpen.Point
. For the sphere 3 points normal method: 1st point sphereDirectionPoint2 is aNXOpen.Point
. For the sphere 3 points normal method: 2nd point sphereDirectionPoint3 is aNXOpen.Point
. For the sphere 3 points normal method: 3rd point flipNormal is a bool. For the sphere 3 points normal method: flag to flip the normal direction refinementLevel is a int. Refinement level of the distributed plave wave set.New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetTargetSetExcludedMembers¶
-
SetManager.
GetTargetSetExcludedMembers
¶ Gets the objects for the specified target set excluded set
Signature
GetTargetSetExcludedMembers(setIndex)
Parameters: setIndex (int) – index of the set Returns: objects in set Return type: list of NXOpen.CAE.SetObject
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetTargetSetGroup¶
-
SetManager.
GetTargetSetGroup
¶ Gets the CAE group in the specified set
Signature
GetTargetSetGroup(setIndex)
Parameters: setIndex (int) – index of the set Returns: group object from set. may be None Return type: NXOpen.CAE.CaeGroup
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetTargetSetMembers¶
-
SetManager.
GetTargetSetMembers
¶ Gets the objects for the specified target set
Signature
GetTargetSetMembers(setIndex)
Parameters: setIndex (int) – index of the set Returns: a tuple Return type: A tuple consisting of (displayCoordinateSystem, objects). displayCoordinateSystem is a NXOpen.NXObject
. display coordinate system objects is a list ofNXOpen.CAE.SetObject
. objects in setNew in version NX4.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetTargetSetPlane¶
-
SetManager.
GetTargetSetPlane
¶ Gets the parameters from a plane target set.
The plane target set is a special type of target set that does not rely on any FEM entities. It is a purely geometric plane defined in space that may or may not touch any elements or nodes. It cannot rely on the standard
CAE.SetManager.CreateCaeSet()
andCAE.CAESet.SetMembers()
since and requires its own interface to retrieve the parameters.Signature
GetTargetSetPlane(setIndex)
Parameters: setIndex (int) – index of the set Returns: a tuple Return type: A tuple consisting of (planePosition, planeNormal). planePosition is a NXOpen.Point3d
. plane’s position planeNormal is aNXOpen.Vector3d
. plane’s normalNew in version NX11.0.0.
Deprecated since version NX12.0.0: Use overloaded
CAE.SetManager.GetTargetSetPlaneWithOffset()
.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetTargetSetPlaneWithOffset¶
-
SetManager.
GetTargetSetPlaneWithOffset
¶ Gets the parameters from a plane target set.
The plane target set is a special type of target set that does not rely on any FEM entities. It is a purely geometric plane defined in space that may or may not touch any elements or nodes. It cannot rely on the standard
CAE.SetManager.CreateCaeSet()
andCAE.CAESet.SetMembers()
since and requires its own interface to retrieve the parameters.Signature
GetTargetSetPlaneWithOffset(setIndex)
Parameters: setIndex (int) – index of the set Returns: a tuple Return type: A tuple consisting of (planePosition, planeNormal, offsetValue). planePosition is a NXOpen.Point3d
. plane’s position planeNormal is aNXOpen.Vector3d
. plane’s normal offsetValue is aNXOpen.Expression
. offset value that was used to construct the plane.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetTargetSetPointLocation¶
-
SetManager.
GetTargetSetPointLocation
¶ Gets the position from a point location target set.
The point location target set is a special type of target set that does not rely on any FEM entities. It is a purely geometric point located in space that may or may not touch any elements or nodes. It cannot rely on the standard
CAE.SetManager.CreateCaeSet()
andCAE.CAESet.SetMembers()
since and requires its own interface to retrieve the position.Signature
GetTargetSetPointLocation(setIndex)
Parameters: setIndex (int) – index of the set Returns: point location’s position Return type: NXOpen.Point3d
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Print¶
-
SetManager.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
SetManager.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetTargetSetDistributedPlanes¶
-
SetManager.
SetTargetSetDistributedPlanes
¶ Sets the parameters for a distributed planes set.
Signature
SetTargetSetDistributedPlanes(setIndex, centerMethod, centerPoint, radiusMethod, radiusFactor, radiusValue, bboxOption, bboxElems, spaceDefinition, sphereDirection, sphereDirectionVector, sphereDirectionPoint1, sphereDirectionPoint2, sphereDirectionPoint3, flipNormal, refinementLevel)
Parameters: - setIndex (int) – Index of the set
- centerMethod (
NXOpen.CAE.SetManagerDistributedPlanesPosition
) – Method used to define the sphere center - centerPoint (
NXOpen.Point
) – Sphere manual center position. - radiusMethod (
NXOpen.CAE.SetManagerDistributedPlanesPosition
) – Method used to define the sphere radius - radiusFactor (
NXOpen.Expression
) – Multiplying factor applied to the model bounding box diagonal to get the sphere radius. - radiusValue (
NXOpen.Expression
) – Radius manual value. - bboxOption (
NXOpen.CAE.SetManagerDistributedPlanesBboxType
) – Bounding box definition option - bboxElems (list of
NXOpen.CAE.FEElement
) – Selection used to calculate the bounding box for the manual bounding box option - spaceDefinition (
NXOpen.CAE.SetManagerDistributedPlanesBoundingSphereType
) – Type of bounding sphere (half or full) - sphereDirection (
NXOpen.CAE.SetManagerDistributedPlanesBoundingSphereDirection
) – Sphere direction definition method - sphereDirectionVector (
NXOpen.Direction
) – For the sphere vector method: sphere direction vector - sphereDirectionPoint1 (
NXOpen.Point
) – For the sphere 3 points normal method: 1st point - sphereDirectionPoint2 (
NXOpen.Point
) – For the sphere 3 points normal method: 2nd point - sphereDirectionPoint3 (
NXOpen.Point
) – For the sphere 3 points normal method: 3rd point - flipNormal (bool) – For the sphere 3 points normal method: flag to flip the normal direction
- refinementLevel (int) – Refinement level of the distributed plave wave set.
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetTargetSetEdgePath¶
-
SetManager.
SetTargetSetEdgePath
¶ Overloaded method SetTargetSetEdgePath
SetTargetSetEdgePath(setIndex, seedEdges, seedVertices)
SetTargetSetEdgePath(setIndex, seedEdges, seedVertices, preferFreeEdges, allowGapJumping, gapJumpingTolerance)
-------------------------------------
Sets the CAE edge path in the specified set
Signature
SetTargetSetEdgePath(setIndex, seedEdges, seedVertices)
Parameters: - setIndex (int) – index of the set
- seedEdges (list of
NXOpen.CAE.CAEEdge
) – seed edges to define the path - seedVertices (list of
NXOpen.CAE.CAEVertex
) – seed vertices to define the path
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use overloaded
CAE.SetManager.SetTargetSetEdgePath()
with additional arguments instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Sets the CAE edge path in the specified set
Signature
SetTargetSetEdgePath(setIndex, seedEdges, seedVertices, preferFreeEdges, allowGapJumping, gapJumpingTolerance)
Parameters: - setIndex (int) – index of the set
- seedEdges (list of
NXOpen.CAE.CAEEdge
) – seed edges to define the path - seedVertices (list of
NXOpen.CAE.CAEVertex
) – seed vertices to define the path - preferFreeEdges (list of bool) – if true for seed, prefer free edges
- allowGapJumping (list of bool) – if true for seed, gaps between edges will be jumped
- gapJumpingTolerance (list of float) – if allowGapJumping is true for seed, this is the tolerance to use for jumping gaps between edges
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
SetTargetSetElemEdgePath¶
-
SetManager.
SetTargetSetElemEdgePath
¶ Overloaded method SetTargetSetElemEdgePath
SetTargetSetElemEdgePath(setIndex, seedEdges, seedVertices)
SetTargetSetElemEdgePath(setIndex, seedEdges, seedVertices, preferFreeEdges, preferGeometryAssociatedEdges, preferFeatureElementEdges, featureAngleTolerance, allowGapJumping, gapJumpingTolerance)
-------------------------------------
Sets the CAE element edge path in the specified set
Signature
SetTargetSetElemEdgePath(setIndex, seedEdges, seedVertices)
Parameters: - setIndex (int) – index of the set
- seedEdges (list of
NXOpen.CAE.FEElemEdge
) – seed element edges to define the path - seedVertices (list of
NXOpen.CAE.FENode
) – seed nodes to define the path
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use overloaded
CAE.SetManager.SetTargetSetElemEdgePath()
with additional arguments instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Sets the CAE element edge path in the specified set
Signature
SetTargetSetElemEdgePath(setIndex, seedEdges, seedVertices, preferFreeEdges, preferGeometryAssociatedEdges, preferFeatureElementEdges, featureAngleTolerance, allowGapJumping, gapJumpingTolerance)
Parameters: - setIndex (int) – index of the set
- seedEdges (list of
NXOpen.CAE.FEElemEdge
) – seed element edges to define the path - seedVertices (list of
NXOpen.CAE.FENode
) – seed nodes to define the path - preferFreeEdges (list of bool) – if true for seed, prefer free element edges
- preferGeometryAssociatedEdges (list of bool) – if true for seed, prefer geometry associated element edges
- preferFeatureElementEdges (list of bool) – if true for seed, prefer feature element edges
- featureAngleTolerance (list of float) – if preferFeatureElementEdge is true for seed, this is the feature angle tolerance to use
- allowGapJumping (list of bool) – if true for seed, gaps between element edges will be jumped
- gapJumpingTolerance (list of float) – if allowGapJumping is true for seed, this is the tolerance to use for jumping gaps between element edges
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
SetTargetSetExcludedMembers¶
-
SetManager.
SetTargetSetExcludedMembers
¶ Overloaded method SetTargetSetExcludedMembers
SetTargetSetExcludedMembers(setIndex, excludedObjects)
SetTargetSetExcludedMembers(setIndex, selRecipeFilter, objects)
-------------------------------------
Sets the CAE objects in the specified target set exclude set
Signature
SetTargetSetExcludedMembers(setIndex, excludedObjects)
Parameters: - setIndex (int) – index of the set
- excludedObjects (list of
NXOpen.CAE.SetObject
) – excluded objects to add to set
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Sets the CAE objects in the specified target set exclude set
Signature
SetTargetSetExcludedMembers(setIndex, selRecipeFilter, objects)
Parameters: - setIndex (int) – index of the set
- selRecipeFilter (
NXOpen.CAE.CaeSetGroupFilterType
) – filter to extract type of objects from the selection recipe - objects (list of
NXOpen.CAE.SetObject
) – excluded objects to add to set
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
SetTargetSetGroup¶
-
SetManager.
SetTargetSetGroup
¶ Sets the CAE group in the specified set
Signature
SetTargetSetGroup(setIndex, filterType, group)
Parameters: - setIndex (int) – index of the set
- filterType (
NXOpen.CAE.CaeSetGroupFilterType
) – filter to extract type of objects from the group - group (
NXOpen.CAE.CaeGroup
) – group to add to set
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetTargetSetMembers¶
-
SetManager.
SetTargetSetMembers
¶ Overloaded method SetTargetSetMembers
SetTargetSetMembers(setIndex, objects)
SetTargetSetMembers(setIndex, selRecipeFilter, objects)
-------------------------------------
Sets the CAE objects in the specified set
Signature
SetTargetSetMembers(setIndex, objects)
Parameters: - setIndex (int) – index of the set
- objects (list of
NXOpen.CAE.SetObject
) – objects to add to set
New in version NX4.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Sets the CAE objects in the specified set
Signature
SetTargetSetMembers(setIndex, selRecipeFilter, objects)
Parameters: - setIndex (int) – index of the set
- selRecipeFilter (
NXOpen.CAE.CaeSetGroupFilterType
) – filter to extract type of objects from the selection recipe - objects (list of
NXOpen.CAE.SetObject
) – objects to add to set
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
SetTargetSetPlane¶
-
SetManager.
SetTargetSetPlane
¶ Creates a plane target set.
The plane target set is a special type of target set that does not rely on any FEM entities. It is a purely geometric plane defined in space that may or may not touch elements or nodes. It cannot rely on the standard
CAE.SetManager.CreateCaeSet()
andCAE.CAESet.SetMembers()
since and requires its own interface to create the plane.Signature
SetTargetSetPlane(setIndex, planePosition, planeNormal)
Parameters: - setIndex (int) – index of the set
- planePosition (
NXOpen.Point3d
) – plane’s position - planeNormal (
NXOpen.Vector3d
) – plane’s normal.
New in version NX11.0.0.
Deprecated since version NX12.0.0: Use overloaded
CAE.SetManager.SetTargetSetPlaneWithOffset()
.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetTargetSetPlaneWithOffset¶
-
SetManager.
SetTargetSetPlaneWithOffset
¶ Creates a plane target set.
The plane target set is a special type of target set that does not rely on any FEM entities. It is a purely geometric plane defined in space that may or may not touch elements or nodes. It cannot rely on the standard
CAE.SetManager.CreateCaeSet()
andCAE.CAESet.SetMembers()
since and requires its own interface to create the plane.Signature
SetTargetSetPlaneWithOffset(setIndex, planePosition, planeNormal, offsetValue)
Parameters: - setIndex (int) – index of the set.
- planePosition (
NXOpen.Point3d
) – plane’s position. - planeNormal (
NXOpen.Vector3d
) – plane’s normal. - offsetValue (
NXOpen.Expression
) – offset value that was used to construct the plane.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetTargetSetPointLocation¶
-
SetManager.
SetTargetSetPointLocation
¶ Creates a point location target set.
The point location target set is a special type of target set that does not rely on any FEM entities. It is a purely geometric point located in space that may or may not touch any elements or nodes. It cannot rely on the standard
CAE.SetManager.CreateCaeSet()
andCAE.CAESet.SetMembers()
since and requires its own interface to create the point location.Signature
SetTargetSetPointLocation(setIndex, position)
Parameters: - setIndex (int) – index of the set
- position (
NXOpen.Point3d
) – point location’s position
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)