NXObject Class¶
-
class
NXOpen.
NXObject
¶ Bases:
NXOpen.TaggedObject
,NXOpen.INXObject
A base class providing low-level services for most NXOpen classes.
For more information on NX rules for Names and Attributes, see the Properties section of the Gateway Help.
This is an abstract class, and cannot be instantiated.
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
NXObjectAttributeType Enumeration | Specifies attribute type. |
NXObjectDateAndTimeFormat Enumeration | Specifies the format of the date and time attribute. |
Structs¶
NXObjectAttributeInformation_Struct Struct | Contains attribute information. |
NXObjectComputationalTime_Struct Struct | Holds the computational time value of a time attribute. |
Property Detail¶
IsOccurrence¶
-
NXObject.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
NXObject.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
NXObject.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
NXObject.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
NXObject.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
NXObject.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
CreateAttributeIterator¶
-
NXObject.
CreateAttributeIterator
¶ Create an attribute iterator
Signature
CreateAttributeIterator()
Returns: A new attribute iterator object Return type: NXOpen.AttributeIterator
New in version NX11.0.0.
License requirements: None.
DeleteAllAttributesByType¶
-
NXObject.
DeleteAllAttributesByType
¶ Overloaded method DeleteAllAttributesByType
DeleteAllAttributesByType(type)
DeleteAllAttributesByType(type, option)
-------------------------------------
Deletes all attributes of a specific type. This method performs an immediate update except when the object is a
NXOpen.Features.Feature
. If a candidate attribute is an array attribute, this method will delete all the array elements. NOTE: If the input specifies reference type, then this function will delete string type non-array attributes that have a reference value. The reference type is used only to single out string type non-array attributes that contain a reference value. The use of reference type in this function is deprecated. Please use string type instead.Signature
DeleteAllAttributesByType(type)
Parameters: type ( NXOpen.NXObjectAttributeType
) –New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
DeleteUserAttributes()
instead.License requirements: None.
-------------------------------------
Deletes all attributes of a specific type with the option to update or not. If a candidate attribute is an array attribute, this method will delete all the array elements. NOTE: If the input specifies reference type, then this function will delete string type non-array attributes that have a reference value. The reference type is used only to single out string type non-array attributes that contain a reference value. The use of reference type in this function is deprecated. Please use string type instead.
Signature
DeleteAllAttributesByType(type, option)
Parameters: - type (
NXOpen.NXObjectAttributeType
) – - option (
NXOpen.UpdateOption
) –
New in version NX5.0.1.
Deprecated since version NX8.0.0: Use
DeleteUserAttributes()
instead.License requirements: None.
-------------------------------------
DeleteAttributeByTypeAndTitle¶
-
NXObject.
DeleteAttributeByTypeAndTitle
¶ Overloaded method DeleteAttributeByTypeAndTitle
DeleteAttributeByTypeAndTitle(type, title)
DeleteAttributeByTypeAndTitle(type, title, option)
-------------------------------------
Deletes an attribute by type and title. This method performs an immediate update except when the object is a
NXOpen.Features.Feature
. If a candidate attribute is an array attribute, this method will delete all the array elements. NOTE: If the input specifies reference type, then this function will delete string type attributes that have a reference value. The reference type is used only to single out string type attributes that contain a reference value. The use of reference type in this function is discouraged.Signature
DeleteAttributeByTypeAndTitle(type, title)
Parameters: - type (
NXOpen.NXObjectAttributeType
) – - title (str) –
New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
DeleteUserAttribute()
instead.License requirements: None.
-------------------------------------
Deletes an attribute by type and title with the option to update or not. If a candidate attribute is an array attribute, this method will delete all the array elements. NOTE: If the input specifies reference type, then this function will delete string type attributes that have a reference value. The reference type is used only to single out string type attributes that contain a reference value. The use of reference type in this function is discouraged.
Signature
DeleteAttributeByTypeAndTitle(type, title, option)
Parameters: - type (
NXOpen.NXObjectAttributeType
) – - title (str) –
- option (
NXOpen.UpdateOption
) –
New in version NX5.0.1.
Deprecated since version NX8.0.0: Use
DeleteUserAttribute()
instead.License requirements: None.
-------------------------------------
DeleteUserAttribute¶
-
NXObject.
DeleteUserAttribute
¶ Deletes the first attribute encountered with the given Type, Title.
If a candidate attribute is not an array attribute, the DeleteEntireArray input is ignored, If a candidate attribute is an array attribute and DeleteEntireArray input is ‘false’, then the last element of the array is deleted. If a candidate attribute is an array attribute and DeleteEntireArray input is ‘true’, then the entire array is deleted. NOTE: This method does not support the use of
NXOpen.NXObjectAttributeType.Reference
.Signature
DeleteUserAttribute(type, title, deleteEntireArray, option)
Parameters: - type (
NXOpen.NXObjectAttributeType
) – - title (str) –
- deleteEntireArray (bool) –
- option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
- type (
DeleteUserAttributes¶
-
NXObject.
DeleteUserAttributes
¶ Overloaded method DeleteUserAttributes
DeleteUserAttributes(iterator, option)
DeleteUserAttributes(type, option)
-------------------------------------
Deletes the attributes on the object, if any, that satisfy the given iterator
Signature
DeleteUserAttributes(iterator, option)
Parameters: - iterator (
NXOpen.AttributeIterator
) –NXOpen.AttributeIterator
- option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Deletes the attributes encountered with the given Type with option to update or not. NOTE: This method does not support the use of
NXOpen.NXObjectAttributeType.Reference
.Signature
DeleteUserAttributes(type, option)
Parameters: - type (
NXOpen.NXObjectAttributeType
) – - option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
-------------------------------------
FindObject¶
-
NXObject.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAttributeTitlesByType¶
-
NXObject.
GetAttributeTitlesByType
¶ Gets all the attribute titles of a specific type.
Only Title and Type are set in the returned struct. No values are returned. Array attributes are supported. The Title returned is the array title, with no index appended. Only one title is returned per array. This function does not return the titles of unset attributes. NOTE: If the input specifies reference type, then this function will get string type attributes that have a reference value. The reference type is used only to single out string type attributes that contain a reference value. The use of reference type in this function is deprecated. Please use string type instead.
Signature
GetAttributeTitlesByType(type)
Parameters: type ( NXOpen.NXObjectAttributeType
) –Returns: Return type: list of NXOpen.NXObjectAttributeInformation_Struct
New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
GetUserAttributes()
instead.License requirements: None.
GetBooleanUserAttribute¶
-
NXObject.
GetBooleanUserAttribute
¶ Gets a boolean attribute by Title and array Index.
This function will not look for unset attributes. If the attribute to be found is not an array, set the Index to -1, otherwise set it to the desired index. The first element of an array has Index 0 (zero). To get all the array elements of an array, please use
NXOpen.NXObject.GetUserAttributes()
.Signature
GetBooleanUserAttribute(title, index)
Parameters: - title (str) –
- index (int) –
Returns: Return type: bool
New in version NX8.0.0.
License requirements: None.
GetComputationalTimeUserAttribute¶
-
NXObject.
GetComputationalTimeUserAttribute
¶ Gets a time attribute by Title and array Index.
The time value returned will be in the current time zone of the machine running the program. If the attribute to be found is not an array, set the Index to -1, otherwise set it to the desired index. The first element of an array has Index 0 (zero). To get all the array elements of an array, please use
NXOpen.NXObject.GetUserAttributes()
.Signature
GetComputationalTimeUserAttribute(title, index)
Parameters: - title (str) –
- index (int) –
Returns: The time in the local time zone
Return type: New in version NX8.5.2.
License requirements: None.
GetIntegerAttribute¶
-
NXObject.
GetIntegerAttribute
¶ Gets an integer attribute by title.
This method does not support array attributes.
Signature
GetIntegerAttribute(title)
Parameters: title (str) – Returns: Return type: int New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
GetUserAttribute()
instead.License requirements: None.
GetIntegerUserAttribute¶
-
NXObject.
GetIntegerUserAttribute
¶ Gets an integer attribute by Title and array Index.
This function will not look for unset attributes. If the attribute to be found is not an array, set the Index to -1, otherwise set it to the desired index. The first element of an array has Index 0 (zero). To get all the array elements of an array, please use
NXOpen.NXObject.GetUserAttributes()
.Signature
GetIntegerUserAttribute(title, index)
Parameters: - title (str) –
- index (int) –
Returns: Return type: int
New in version NX8.0.0.
License requirements: None.
GetNextUserAttribute¶
-
NXObject.
GetNextUserAttribute
¶ Gets the next attribute encountered on the object, if any, that satisfies the given iterator.
Signature
GetNextUserAttribute(iterator)
Parameters: iterator ( NXOpen.AttributeIterator
) –NXOpen.AttributeIterator
Returns: a tuple Return type: A tuple consisting of (foundAttribute, info). foundAttribute is a bool. info is a NXOpen.NXObjectAttributeInformation_Struct
.New in version NX11.0.0.
License requirements: None.
GetPdmReferenceAttributeValue¶
-
NXObject.
GetPdmReferenceAttributeValue
¶ Gets the value of PDM Reference attribute for given object.
User should provide attribute title and displayed value will be returned.
Signature
GetPdmReferenceAttributeValue(attributeTitle)
Parameters: attributeTitle (str) – Returns: Return type: str New in version NX12.0.0.
License requirements: None.
GetRealAttribute¶
-
NXObject.
GetRealAttribute
¶ Gets a real attribute by title.
This method does not support array attributes.
Signature
GetRealAttribute(title)
Parameters: title (str) – Returns: Return type: float New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
GetUserAttribute()
instead.License requirements: None.
GetRealUserAttribute¶
-
NXObject.
GetRealUserAttribute
¶ Gets a real attribute by Title and array Index.
This function will not look for unset attributes. If the attribute to be found is not an array, set the Index to -1, otherwise set it to the desired index. The first element of an array has Index 0 (zero). To get all the array elements of an array, please use
NXOpen.NXObject.GetUserAttributes()
.Signature
GetRealUserAttribute(title, index)
Parameters: - title (str) –
- index (int) –
Returns: Return type: float
New in version NX8.0.0.
License requirements: None.
GetReferenceAttribute¶
-
NXObject.
GetReferenceAttribute
¶ Gets the reference string (not the calculated value) of a string attribute that uses a reference string.
Get the attribute by title. For the calculated value, please use
NXOpen.NXObject.GetUserAttribute()
This method does not support array attributes.Signature
GetReferenceAttribute(title)
Parameters: title (str) – Returns: Return type: str New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
GetUserAttribute()
instead.License requirements: None.
GetStringAttribute¶
-
NXObject.
GetStringAttribute
¶ Gets a string attribute value by title.
For string attributes that use reference strings, this function returns the calculated value, not the reference string. This method does not support array attributes.
Signature
GetStringAttribute(title)
Parameters: title (str) – Returns: Return type: str New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
GetUserAttribute()
instead.License requirements: None.
GetStringUserAttribute¶
-
NXObject.
GetStringUserAttribute
¶ Gets a string attribute by Title and array Index.
For reference type string attributes, the calculated StringValue is returned. This function will not look for unset attributes. If the attribute to be found is not an array, set the Index to -1, otherwise set it to the desired index. The first element of an array has Index 0 (zero). To get all the array elements of an array, please use
NXOpen.NXObject.GetUserAttributes()
.Signature
GetStringUserAttribute(title, index)
Parameters: - title (str) –
- index (int) –
Returns: Return type: str
New in version NX8.0.0.
License requirements: None.
GetTimeAttribute¶
-
NXObject.
GetTimeAttribute
¶ Gets a time attribute by title.
The time returned will be in the current time zone of the machine running the program. This method does not support array attributes. This method is deprecated.
Signature
GetTimeAttribute(format, title)
Parameters: - format (
NXOpen.NXObjectDateAndTimeFormat
) – - title (str) –
Returns: Return type: str
New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
GetUserAttribute()
instead.License requirements: None.
- format (
GetTimeUserAttribute¶
-
NXObject.
GetTimeUserAttribute
¶ Gets a time attribute by Title and array Index.
The date format set by the Customer Defaults is used. The time value returned is in the current time zone of the machine running the program. This function will not look for unset attributes. If the attribute to be found is not an array, set the Index to -1, otherwise set it to the desired index. The first element of an array has Index 0 (zero). To get all the array elements of an array, please use
NXOpen.NXObject.GetUserAttributes()
. NOTE: The returned string must be deleted by the callerSignature
GetTimeUserAttribute(title, index)
Parameters: - title (str) –
- index (int) –
Returns: Return type: str
New in version NX8.0.0.
License requirements: None.
GetUserAttribute¶
-
NXObject.
GetUserAttribute
¶ Overloaded method GetUserAttribute
GetUserAttribute(title, type, index)
GetUserAttribute(title, includeUnset, addStringValues, type)
-------------------------------------
Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. This function will return data for unset attributes. For non-string attribute types, the string-converted value is returned as well for convenience. If the attribute to be found is not an array, set the Index to -1, otherwise set it to the desired index. If an unset attribute is read, then the index returned has no meaning. The first element of an array has Index 0 (zero). To get all the array elements of an array, please use
NXOpen.NXObject.GetUserAttributes()
. The date format set by the Customer Defaults is used for attributes of type time. NOTE: This method does not support the use ofNXOpen.NXObjectAttributeType.Reference
. Instead, useNXOpen.NXObjectAttributeType.String
. For reference type string attributes, both the ReferenceValue and the calculated StringValue are returned.Signature
GetUserAttribute(title, type, index)
Parameters: - title (str) –
- type (
NXOpen.NXObjectAttributeType
) – - index (int) –
Returns: Return type: New in version NX8.0.0.
License requirements: None.
-------------------------------------
Gets the first attribute (or attribute array) encountered on the object, if any, with a given Title and Type. This function will optionally return data for unset attributes. For non-string attribute types, the string-converted value is returned as well for convenience. If the attribute cannot be found, but a template is found, then a single struct is returned with information from the template. If neither an attribute nor a template can be found, then no struct is returned (None)). If a non-array attribute is found, a single struct is returned with information from that attribute. If an array attribute is found, then an array of structs is returned with information from each of the array elements of the attribute. Array elements are returned in order of increasing indices. The first element of an array has Index 0 (zero). The date format set by the Customer Defaults is used for attributes of type time. NOTE: This method does not support the use of
NXOpen.NXObjectAttributeType.Reference
. Instead, useNXOpen.NXObjectAttributeType.String
. For reference type string attributes, both the ReferenceValue and the calculated StringValue are returned.Signature
GetUserAttribute(title, includeUnset, addStringValues, type)
Parameters: - title (str) –
- includeUnset (bool) –
- addStringValues (bool) –
- type (
NXOpen.NXObjectAttributeType
) –
Returns: Return type: New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
GetUserAttribute()
instead.License requirements: None.
-------------------------------------
GetUserAttributeAsString¶
-
NXObject.
GetUserAttributeAsString
¶ Gets the first attribute encountered on the object, if any, with a given title, type and array index.
The value of the attribute is converted to and returned as a string. If the attribute is not an array, the Index is ignored (if this is known beforehand, we recommend setting the Index to -1 to save time). The first element of an array has Index 0 (zero). To get all the array elements of an array, please use
NXOpen.NXObject.GetUserAttributes()
. The date format set by the Customer Defaults is used for attributes of type time. NOTE: This method does not support the use ofNXOpen.NXObjectAttributeType.Reference
. Instead, useNXOpen.NXObjectAttributeType.String
. For reference type string attributes, the calculated StringValue is returned.Signature
GetUserAttributeAsString(title, type, index)
Parameters: - title (str) –
- type (
NXOpen.NXObjectAttributeType
) – - index (int) –
Returns: Return type: str
New in version NX8.0.0.
License requirements: None.
GetUserAttributeCount¶
-
NXObject.
GetUserAttributeCount
¶ Overloaded method GetUserAttributeCount
GetUserAttributeCount(iterator)
GetUserAttributeCount(iterator, countArrayAsOneAttribute)
GetUserAttributeCount(type)
GetUserAttributeCount(type, includeUnset, countArrayAsOneAttribute)
-------------------------------------
Gets the count of set attributes on the object, if any, that satisfy the given iterator. Array elements are counted individually.
Signature
GetUserAttributeCount(iterator)
Parameters: iterator ( NXOpen.AttributeIterator
) –NXOpen.AttributeIterator
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Gets the count of set attributes on the object, if any, that satisfy the given iterator. Array elements are optionally counted individually.
Signature
GetUserAttributeCount(iterator, countArrayAsOneAttribute)
Parameters: - iterator (
NXOpen.AttributeIterator
) –NXOpen.AttributeIterator
- countArrayAsOneAttribute (bool) –
Returns: Return type: int
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Gets the count of set attributes on the object, if any, of the given type. Will not include unset attributes. Array elements are counted individually.
Signature
GetUserAttributeCount(type)
Parameters: type ( NXOpen.NXObjectAttributeType
) –Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Gets the count of attributes on the object, if any, of the given type. Includes option to include unset attributes (i.e. to count attribute templates with no associated attributes). Includes option to count arrays as one attribute or to count array elements individually. NOTE: This method does not support the use of
NXOpen.NXObjectAttributeType.Reference
. Instead, useNXOpen.NXObjectAttributeType.String
.Signature
GetUserAttributeCount(type, includeUnset, countArrayAsOneAttribute)
Parameters: - type (
NXOpen.NXObjectAttributeType
) – - includeUnset (bool) –
- countArrayAsOneAttribute (bool) –
Returns: Return type: int
New in version NX10.0.0.
License requirements: None.
-------------------------------------
GetUserAttributeLock¶
-
NXObject.
GetUserAttributeLock
¶ Determine the lock of the given attribute.
For array attributes, the Title should be set to the array title, without the appended index. Individual array elements cannot be separately locked
Signature
GetUserAttributeLock(title, type)
Parameters: - title (str) –
- type (
NXOpen.NXObjectAttributeType
) –
Returns: Return type: bool
New in version NX8.0.0.
License requirements: None.
GetUserAttributeSize¶
-
NXObject.
GetUserAttributeSize
¶ Gets the size of the first attribute encountered on the object, if any, with a given Title and Type.
For unset attributes (with or without templates), the returned size will be 0. For non-array set attributes, the returned size will be 1. For array attributes, the returned size will be the count of array elements that have been set. NOTE: This method does not support the use of
NXOpen.NXObjectAttributeType.Reference
. Instead, useNXOpen.NXObjectAttributeType.String
.Signature
GetUserAttributeSize(title, type)
Parameters: - title (str) –
- type (
NXOpen.NXObjectAttributeType
) –
Returns: Return type: int
New in version NX10.0.0.
License requirements: None.
GetUserAttributeSourceObjects¶
-
NXObject.
GetUserAttributeSourceObjects
¶ Returns an array of objects from which this object presents attributes.
The order of the array is in inheritance order so earlier objects may be able to override objects at higher indices in the array allowing for the rules set up for the particular attributes involved. If this object itself can own attributes it will also be in the array.
Signature
GetUserAttributeSourceObjects()
Returns: Return type: list of NXOpen.NXObject
New in version NX8.5.0.
License requirements: None.
GetUserAttributes¶
-
NXObject.
GetUserAttributes
¶ Overloaded method GetUserAttributes
GetUserAttributes(iterator)
GetUserAttributes()
GetUserAttributes(includeUnset)
GetUserAttributes(includeUnset, addStringValues)
-------------------------------------
Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. The results will not include information from associated attribute templates of unset attributes. The elements of array attributes are returned individually in order of increasing indices. The returned Title of an array element is the array title (without index). The Index data member holds the index. The date format set by the Customer Defaults is used. Reference type attributes are returned as being of type
NXOpen.NXObjectAttributeType.String
, and both the ReferenceValue and the calculated StringValue are returned.Signature
GetUserAttributes(iterator)
Parameters: iterator ( NXOpen.AttributeIterator
) –NXOpen.AttributeIterator
Returns: Return type: list of NXOpen.NXObjectAttributeInformation_Struct
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Gets all the attributes that have been set on the given object. The results will not include information from associated attribute templates of unset attributes. The elements of array attributes are returned individually in order of increasing indices. The returned Title of an array element is the array title (without index). The Index data member holds the index. The date format set by the Customer Defaults is used. Reference type attributes are returned as being of type
NXOpen.NXObjectAttributeType.String
, and both the ReferenceValue and the calculated StringValue are returned.Signature
GetUserAttributes()
Returns: Return type: list of NXOpen.NXObjectAttributeInformation_Struct
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Gets all the attributes of the given object. Includes option to return information also from associated attribute templates of unset attributes. The values returned for unset attributes are the default values from the templates. The elements of array attributes are returned individually in order of increasing indices. The returned Title of an array element is the array title (without index). The Index data member holds the index. The date format set by the Customer Defaults is used. Reference type attributes are returnes as being of type
NXOpen.NXObjectAttributeType.String
, and both the ReferenceValue and the calculated StringValue are returned.Signature
GetUserAttributes(includeUnset)
Parameters: includeUnset (bool) – Returns: Return type: list of NXOpen.NXObjectAttributeInformation_Struct
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Gets all the attributes of the given object. Includes option to return information also from associated attribute templates of unset attributes. The values returned for unset attributes are the default values from the templates. Includes an option to return the value not only in the natural type, but also converted to a string (effective only for non-string attributes). The elements of array attributes are returned individually in order of increasing indices. The returned Title of an array element is the array title (without index). The Index data member holds the index. The date format set by the Customer Defaults is used. Reference type attributes are returned as being of type
NXOpen.NXObjectAttributeType.String
, and both the ReferenceValue and the calculated StringValue are returned.Signature
GetUserAttributes(includeUnset, addStringValues)
Parameters: - includeUnset (bool) –
- addStringValues (bool) –
Returns: Return type: New in version NX8.5.0.
Deprecated since version NX11.0.0: Use
GetUserAttributes()
instead.License requirements: None.
-------------------------------------
GetUserAttributesAsStrings¶
-
NXObject.
GetUserAttributesAsStrings
¶ Gets all the attributes that have been set on the given object.
The values are returned as strings. The elements of array attributes are returned individually in order of increasing indices. The returned Title of an array element is the array title (without index). The Index data member holds the index. Reference type attributes return the calculated StringValue. The date format set by the Customer Defaults is used.
Signature
GetUserAttributesAsStrings()
Returns: Return type: list of str New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
GetUserAttributes()
instead.License requirements: None.
HasUserAttribute¶
-
NXObject.
HasUserAttribute
¶ Overloaded method HasUserAttribute
HasUserAttribute(iterator)
HasUserAttribute(title, type, index)
-------------------------------------
Determines if an attribute exists on the object, that satisfies the given iterator
Signature
HasUserAttribute(iterator)
Parameters: iterator ( NXOpen.AttributeIterator
) –NXOpen.AttributeIterator
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. If the attribute to be found is not an array, set the index to -1, otherwise set it to the desired index. The first element of an array has Index 0 (zero). NOTE: This method does not support the use of
NXOpen.NXObjectAttributeType.Reference
. Instead, useNXOpen.NXObjectAttributeType.String
.Signature
HasUserAttribute(title, type, index)
Parameters: - title (str) –
- type (
NXOpen.NXObjectAttributeType
) – - index (int) –
Returns: Return type: bool
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Print¶
-
NXObject.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetAttribute¶
-
NXObject.
SetAttribute
¶ Overloaded method SetAttribute
SetAttribute(title, value)
SetAttribute(title, value, option)
SetAttribute(title, value)
SetAttribute(title, value, option)
SetAttribute(title, value)
SetAttribute(title, value, option)
SetAttribute(title)
SetAttribute(title, option)
-------------------------------------
Creates or modifies an integer attribute. This method performs an immediate update except when the object is a
NXOpen.Features.Feature
. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.Signature
SetAttribute(title, value)
Parameters: - title (str) –
- value (int) –
New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
Creates or modifies an integer attribute with the option to update or not. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetAttribute(title, value, option)
Parameters: - title (str) –
- value (int) –
- option (
NXOpen.UpdateOption
) –
New in version NX5.0.1.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
Creates or modifies a real attribute. This method performs an immediate update except when the object is a
NXOpen.Features.Feature
. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.Signature
SetAttribute(title, value)
Parameters: - title (str) –
- value (float) –
New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
Creates or modifies a real attribute with the option to update or not. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetAttribute(title, value, option)
Parameters: - title (str) –
- value (float) –
- option (
NXOpen.UpdateOption
) –
New in version NX5.0.1.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
Creates or modifies a string attribute. This method performs an immediate update except when the object is a
NXOpen.Features.Feature
. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.Signature
SetAttribute(title, value)
Parameters: - title (str) –
- value (str) –
New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
Creates or modifies a string attribute with the option to update or not. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetAttribute(title, value, option)
Parameters: - title (str) –
- value (str) –
- option (
NXOpen.UpdateOption
) –
New in version NX5.0.1.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
Creates or modifies a null attribute which is an attribute with a title and no value. This method performs an immediate update except when the object is a
NXOpen.Features.Feature
. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.Signature
SetAttribute(title)
Parameters: title (str) – New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
Creates or modifies a null attribute with the option to update or not. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetAttribute(title, option)
Parameters: - title (str) –
- option (
NXOpen.UpdateOption
) –
New in version NX5.0.1.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
SetBooleanUserAttribute¶
-
NXObject.
SetBooleanUserAttribute
¶ Creates or modifies a boolean attribute with the option to update or not.
To set a non-array attribute, set the index = -1. Arrays can be extended only one element at a time. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetBooleanUserAttribute(title, index, value, option)
Parameters: - title (str) –
- index (int) –
- value (bool) –
- option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
SetName¶
-
NXObject.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetPdmReferenceAttribute¶
-
NXObject.
SetPdmReferenceAttribute
¶ Sets the value of PDM Reference attribute on the object.
User should provide attribute title and alias value that is displayed on UI. If reference attribute is of Array type it will be ignored. Alias string will be converted to internal value (i.e. session identifier) and internal value will be set on given object.
Signature
SetPdmReferenceAttribute(attributeTitle, attributeValue)
Parameters: - attributeTitle (str) –
- attributeValue (str) –
New in version NX12.0.0.
License requirements: None.
SetReferenceAttribute¶
-
NXObject.
SetReferenceAttribute
¶ Overloaded method SetReferenceAttribute
SetReferenceAttribute(title, value)
SetReferenceAttribute(title, value, option)
-------------------------------------
Creates or modifies a string attribute which uses a reference string. This method performs an immediate update except when the object is a
NXOpen.Features.Feature
. NOTE: The input value must be a valid reference string. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.Signature
SetReferenceAttribute(title, value)
Parameters: - title (str) –
- value (str) –
New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
Creates or modifies a string attribute which uses a reference string, with the option to update or not. NOTE: The input value must be a valid reference string. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetReferenceAttribute(title, value, option)
Parameters: - title (str) –
- value (str) –
- option (
NXOpen.UpdateOption
) –
New in version NX5.0.1.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
SetTimeAttribute¶
-
NXObject.
SetTimeAttribute
¶ Overloaded method SetTimeAttribute
SetTimeAttribute(title, value)
SetTimeAttribute(title, value, option)
-------------------------------------
Creates or modifies a time attribute. This method performs an immediate update except when the object is a
NXOpen.Features.Feature
. The time value is assumed to be in the current time zone of the machine running the program. NX will store the value in UTC. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.Signature
SetTimeAttribute(title, value)
Parameters: - title (str) –
- value (str) – The current date and time is used if the value is None. See
NXOpen.NXObjectDateAndTimeFormat
for valid formats.
New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
Creates or modifies a time attribute with the option to update or not. The time value is assumed to be in the current time zone of the machine running the program. NX will store the value in UTC. This method does not support array attributes. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetTimeAttribute(title, value, option)
Parameters: - title (str) –
- value (str) – The current date and time is used if the value is None. See
NXOpen.NXObjectDateAndTimeFormat
for valid formats. - option (
NXOpen.UpdateOption
) –
New in version NX5.0.1.
Deprecated since version NX8.0.0: Use
SetUserAttribute()
instead.License requirements: None.
-------------------------------------
SetTimeUserAttribute¶
-
NXObject.
SetTimeUserAttribute
¶ Overloaded method SetTimeUserAttribute
SetTimeUserAttribute(title, index, value, option)
SetTimeUserAttribute(title, index, value, option)
-------------------------------------
Creates or modifies a time attribute with the option to update or not. The time value is assumed to be in the current time zone of the machine running the program. NX will store the value in UTC. To set a non-array attribute, set the index = -1. Arrays can be extended only one element at a time. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated. NOTE: The valid range for attributes of type date is from 01-Jan-1970 to 31-Dec-2105
Signature
SetTimeUserAttribute(title, index, value, option)
Parameters: - title (str) –
- index (int) –
- value (str) – The current date and time is used if the value is None. See
NXOpen.NXObjectDateAndTimeFormat
for valid formats. - option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Creates or modifies a time attribute with the option to update or not. The time value is assumed to be in the current time zone of the machine running the program. NX will store the value in UTC. To set a non-array attribute, set the index = -1. Arrays can be extended only one element at a time. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetTimeUserAttribute(title, index, value, option)
Parameters: - title (str) –
- index (int) –
- value (
NXOpen.NXObjectComputationalTime_Struct
) – The current date and time is used if the value is (0,0). - option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
-------------------------------------
SetUserAttribute¶
-
NXObject.
SetUserAttribute
¶ Overloaded method SetUserAttribute
SetUserAttribute(info, option)
SetUserAttribute(title, index, value, option)
SetUserAttribute(title, index, value, option)
SetUserAttribute(title, index, value, option)
SetUserAttribute(title, index, option)
-------------------------------------
Creates or modifies an attribute with the option to update or not. NOTE: This method does not support the use of
NXOpen.NXObjectAttributeType.Reference
. Instead, set the type toNXOpen.NXObjectAttributeType.String
and specify a ReferenceValue. NOTE: To set anNXOpen.NXObjectAttributeType.Time
attribute, either a formatted string or a computational value may be used. If both are set (the string is not None and the computational value is not (0,0)), then the computational value will take precedence. The time value in either case is in the current time zone of the machine running the program.The following data members of the Info structure are ignored by this method: Alias Inherited Required Unset Locked OwnedBySystem PdmBased
The following data members of an attribute cannot be edited once the attribute is set: Type Title TitleAlias Array ArrayElementIndex The dimensionality of the Unit specification (cannot change from mm to microA, but from mm to cm is fine)
The following data of an attribute can be set if and only if the attribute is not associated with a template. It cannot be modified once set. Array Category Transient
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated. NOTE: The valid range for attributes of type date is from 01-Jan-1970 to 31-Dec-2105
Signature
SetUserAttribute(info, option)
Parameters: - info (
NXOpen.NXObjectAttributeInformation_Struct
) – - option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Creates or modifies an integer attribute with the option to update or not. To set a non-array attribute, set the index = -1. Arrays can be extended only one element at a time. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetUserAttribute(title, index, value, option)
Parameters: - title (str) –
- index (int) –
- value (int) –
- option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Creates or modifies a real attribute with the option to update or not. To set a non-array attribute, set the index = -1. Arrays can be extended only one element at a time. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetUserAttribute(title, index, value, option)
Parameters: - title (str) –
- index (int) –
- value (float) –
- option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Creates or modifies a string attribute with the option to update or not. To set a non-array attribute, set the index = -1. Arrays can be extended only one element at a time. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetUserAttribute(title, index, value, option)
Parameters: - title (str) –
- index (int) –
- value (str) –
- option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Creates or modifies a null attribute with the option to update or not. To set a non-array attribute, set the index = -1. Arrays can be extended only one element at a time. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetUserAttribute(title, index, option)
Parameters: - title (str) –
- index (int) –
- option (
NXOpen.UpdateOption
) –
New in version NX8.0.0.
License requirements: None.
-------------------------------------
SetUserAttributeLock¶
-
NXObject.
SetUserAttributeLock
¶ Lock or unlock the given attribute.
For array attributes, the Title should be set to the array title, without the appended index. Individual array elements cannot be separately locked. NOTE: Attributes that are reserved (OwnedBySystem), cannot be unlocked. NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetUserAttributeLock(title, type, lock)
Parameters: - title (str) –
- type (
NXOpen.NXObjectAttributeType
) – - lock (bool) –
New in version NX8.0.0.
License requirements: None.