NXObjectDateAndTimeFormat Enumeration¶
NXOpen.NXObject.DateAndTimeFormat is an alias for NXOpen.NXObjectDateAndTimeFormat
-
class
NXOpen.
NXObjectDateAndTimeFormat
¶ Bases:
object
Specifies the format of the date and time attribute.
Enum Members
Enum Member Enum Member Description Numeric 2004/04/28 22:06:15 Textual 28-Apr-2004 22:06:15 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-