CaeGroup Class¶
-
class
NXOpen.CAE.
CaeGroup
¶ Bases:
NXOpen.NXObject
,NXOpen.CAE.IExportableFEEntity
Represents a group class
NXOpen.CAE.CaeGroup
.To obtain an instance of this object use on of the creator in
NXOpen.CAE.CaeGroupCollection
.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Label | Returns or sets the Group Label |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddEntities | Adds entities in to the group |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetElementEdges | Returns Element Edges in the Group. |
GetElementFaces | Returns Element Faces in the Group. |
GetEntities | Gets entities in to the group. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetName | Gets the name of the CaeGroup |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSolverCardSyntax | Returns the solver card syntax strings for this entity. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GroupInformation | Display information of this group |
HasNonDisplayableEntities | Returns whether the group has non-displayable entities |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
HideGroup | Hide this group. |
Prints a representation of this object to the system log file. | |
RemoveEntities | Removes entities from the group |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetEntities | Set entities in to the group |
SetName | CaeGroups the name of the group |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
ShowGroup | Show this group. |
ShowOnlyGroup | Shows this group only. |
Property Detail¶
IsOccurrence¶
-
CaeGroup.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CaeGroup.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Label¶
-
CaeGroup.
Label
¶ Returns or sets the Group Label
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: int New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (int) – The group label must be >=0 and be unique New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Name¶
-
CaeGroup.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CaeGroup.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CaeGroup.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
CaeGroup.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddEntities¶
-
CaeGroup.
AddEntities
¶ Adds entities in to the group
Signature
AddEntities(objects)
Parameters: objects (list of NXOpen.TaggedObject
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
CaeGroup.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetElementEdges¶
-
CaeGroup.
GetElementEdges
¶ Returns Element Edges in the Group.
Signature
GetElementEdges()
Returns: element edges in group Return type: list of NXOpen.CAE.ElemEdgefaceObject
New in version NX11.0.0.
License requirements: None.
GetElementFaces¶
-
CaeGroup.
GetElementFaces
¶ Returns Element Faces in the Group.
Signature
GetElementFaces()
Returns: element edges in group Return type: list of NXOpen.CAE.ElemEdgefaceObject
New in version NX11.0.0.
License requirements: None.
GetEntities¶
-
CaeGroup.
GetEntities
¶ Gets entities in to the group.
Signature
GetEntities()
Returns: Return type: list of NXOpen.TaggedObject
New in version NX6.0.0.
License requirements: None.
GetName¶
-
CaeGroup.
GetName
¶ Gets the name of the CaeGroup
Signature
GetName()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
GetSolverCardSyntax¶
-
CaeGroup.
GetSolverCardSyntax
¶ Returns the solver card syntax strings for this entity.
Signature
GetSolverCardSyntax()
Returns: Return type: list of str New in version NX8.5.0.
License requirements: None.
GroupInformation¶
-
CaeGroup.
GroupInformation
¶ Display information of this group
Signature
GroupInformation()
New in version NX6.0.0.
License requirements: None.
HasNonDisplayableEntities¶
-
CaeGroup.
HasNonDisplayableEntities
¶ Returns whether the group has non-displayable entities
Signature
HasNonDisplayableEntities()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
HideGroup¶
-
CaeGroup.
HideGroup
¶ Hide this group.
Note that
CAE.FEElemEdge
,CAE.FEElemFace
andCAE.CAEEdge
do not participate in this command. They are non-displayable entities and are never drawn individually in NX. UseNXOpen.CAE.CaeGroup.HasNonDisplayableEntities()
to determine if the group contains these entities.Signature
HideGroup()
New in version NX6.0.0.
License requirements: None.
Print¶
-
CaeGroup.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveEntities¶
-
CaeGroup.
RemoveEntities
¶ Removes entities from the group
Signature
RemoveEntities(objects)
Parameters: objects (list of NXOpen.TaggedObject
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetEntities¶
-
CaeGroup.
SetEntities
¶ Set entities in to the group
Signature
SetEntities(objects)
Parameters: objects (list of NXOpen.TaggedObject
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetName¶
-
CaeGroup.
SetName
¶ CaeGroups the name of the group
Signature
SetName(name)
Parameters: name (str) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ShowGroup¶
-
CaeGroup.
ShowGroup
¶ Show this group.
Note that
CAE.FEElemEdge
,CAE.FEElemFace
andCAE.CAEEdge
do not participate in this command. They are non-displayable entities and are never drawn individually in NX. UseNXOpen.CAE.CaeGroup.HasNonDisplayableEntities()
to determine if the group contains these entities.Signature
ShowGroup()
New in version NX6.0.0.
License requirements: None.
ShowOnlyGroup¶
-
CaeGroup.
ShowOnlyGroup
¶ Shows this group only.
Note that
CAE.FEElemEdge
,CAE.FEElemFace
andCAE.CAEEdge
do not participate in this command. They are non-displayable entities and are never drawn individually in NX. UseNXOpen.CAE.CaeGroup.HasNonDisplayableEntities()
to determine if the group contains these entities.Signature
ShowOnlyGroup()
New in version NX6.0.0.
License requirements: None.