SetManagerDistributedPlanesBboxType Enumeration¶
NXOpen.CAE.SetManager.DistributedPlanesBboxType is an alias for NXOpen.CAE.SetManagerDistributedPlanesBboxType
-
class
NXOpen.CAE.
SetManagerDistributedPlanesBboxType
¶ Bases:
object
Used to specify which bounding box defines the position or radius of the sphere
Enum Members
Enum Member Enum Member Description Model the whole FE model is used to calculate the bounding box Selection a selection of elements is used to define the bounding box -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-