CaeSetGroupFilterType Enumeration¶
-
class
NXOpen.CAE.
CaeSetGroupFilterType
¶ Bases:
object
Used to specify the filter to extract type of objects from a group e.g geometric face, element, node ..etc Enum Members
Enum Member Enum Member Description Node filter type is node Element fitler type is any element GeomFace filter type is geometric face GeomBody filter type is geometric body GeomCurve filter type is geometric curve GeomPoint filter type is geometric point PointElement filter type is 0D element BeamElement filter type is 1D element ShellElement filter type is 2D element SolidElement filter type is 3D element GeomPlanarFace filter type is geometric planar face GeomCylFace filter type is geometric cylindrical face BeamElementTypeBar filter type is 1D element of type Bar BeamElementTypeBeam filter type is 1D element of type Beam BeamElementTypeRod filter type is 1D element of type Rod BeamElementTypeBearing filter type is 1D element of type Bearing NodeAndElement filter type is any node and element CaeGeometry filter type is any cae geometry CaeMesh filter type is any cae mesh BoundingVolume filter type is any bounding volume ElementFace filter type is element face ElementEdge filter type is element edge GeomEdge filter type is geometry edge GeomCircularedge filter type is geometry edge BeamElementTypeMpc filter type is 1D element of type MPC CaePointMesh filter type is 0D cae mesh CaeBeamMesh filter type is 1D cae mesh CaeShellMesh filter type is 2D cae mesh CaeSolidMesh filter type is 3D cae mesh BeamMeshTypeBar filter type is 1D mesh of type Bar BeamMeshTypeBeam filter type is 1D mesh of type Beam BeamMeshTypeRod filter type is 1D mesh of type Rod BeamMeshTypeBearing filter type is 1D mesh of type Bearing BeamMeshTypeMpc filter type is 1D mesh of type MPC GeomVertex filter type is geometry vertex FeEntity filter type is any FE entity - node, element, element edge and element face -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-