SetManagerDistributedPlanesPosition Enumeration¶
NXOpen.CAE.SetManager.DistributedPlanesPosition is an alias for NXOpen.CAE.SetManagerDistributedPlanesPosition
-
class
NXOpen.CAE.
SetManagerDistributedPlanesPosition
¶ Bases:
object
Used to specify the method to define the position or the radius of the sphere
Enum Members
Enum Member Enum Member Description Bbox the position or radius is based on the bounding box Manual the position or radius is manually defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-