FEElemEdge Class¶
-
class
NXOpen.CAE.
FEElemEdge
¶ Bases:
NXOpen.TaggedObject
Represents a Finite Element Edge which can be shared by more that one element.
New in version NX7.5.2.
Methods¶
Method | Description |
---|---|
GetElementsAndEdgeIds | Returns the elements for this element edge and the corresponding element edge ids. |
Method Detail¶
GetElementsAndEdgeIds¶
-
FEElemEdge.
GetElementsAndEdgeIds
¶ Returns the elements for this element edge and the corresponding element edge ids.
More information can be queried for these element edges by using the method on
NXOpen.CAE.FEElement
classSignature
GetElementsAndEdgeIds()
Returns: a tuple Return type: A tuple consisting of (ptIElems, edgeIds). ptIElems is a list of NXOpen.CAE.FEElement
. edgeIds is a list of int.New in version NX11.0.0.
License requirements: None.