SetManagerDistributedPlanesBoundingSphereDirection Enumeration¶
NXOpen.CAE.SetManager.DistributedPlanesBoundingSphereDirection is an alias for NXOpen.CAE.SetManagerDistributedPlanesBoundingSphereDirection
-
class
NXOpen.CAE.
SetManagerDistributedPlanesBoundingSphereDirection
¶ Bases:
object
Used to specify the method to define the Z+ direction of the sphere
Enum Members
Enum Member Enum Member Description Vector defines Z+ with a vector ThreePointsNormal defines Z+ from 3 points that form a plane and a normal -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-