TBSTopologyRestrictAreaBuilderCheckTypeOption Enumeration¶
NXOpen.CAE.Optimization.TBSTopologyRestrictAreaBuilder.CheckTypeOption is an alias for NXOpen.CAE.Optimization.TBSTopologyRestrictAreaBuilderCheckTypeOption
-
class
NXOpen.CAE.Optimization.
TBSTopologyRestrictAreaBuilderCheckTypeOption
¶ Bases:
object
Defines the type of restriction
Enum Members
Enum Member Enum Member Description Frozen All elements of the element group which do not undergo any changes during optimization LinkTopo Definition of symmetry and link condtions MaximumsSize Defition of the maximum structural diameter MinimumSize Definition of minimum structural diameter Cast Manufacturing restrictions to guarantee the manufacturing of the elements -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-