TBSOptimizationSolutionCollection Class¶
-
class
NXOpen.CAE.Optimization.
TBSOptimizationSolutionCollection
¶ Bases:
object
Represents a collection of
NXOpen.CAE.Optimization.TBSOptimizationSolution
To obtain an instance of this class, refer to
NXOpen.CAE.Optimization.TBSOptimizationManager
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CloneSolution | Clones an optimization solution and the associated result file optional |
FindObject | Finds an optimization solution with specified name |
Method Detail¶
CloneSolution¶
-
TBSOptimizationSolutionCollection.
CloneSolution
¶ Clones an optimization solution and the associated result file optional
Signature
CloneSolution(sourceSolution, cloneResult)
Parameters: - sourceSolution (
NXOpen.CAE.Optimization.TBSOptimizationSolution
) – - cloneResult (bool) – true if you want associated result files to be cloned as well
Returns: Return type: New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
- sourceSolution (
FindObject¶
-
TBSOptimizationSolutionCollection.
FindObject
¶ Finds an optimization solution with specified name
Signature
FindObject(solutionName)
Parameters: solutionName (str) – Returns: Return type: NXOpen.CAE.Optimization.TBSOptimizationSolution
New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)