TBSOptimizationSolution Class¶
-
class
NXOpen.CAE.Optimization.
TBSOptimizationSolution
¶ Bases:
NXOpen.NXObject
Represents the solution to contain optimization setting
This is an abstract class, and cannot be created.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ControlParameters | Returns the parameters to control optimization |
DesignArea | Returns the design area that will be modified during optimization |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
Objectives | Returns the objective function of the optimization |
OutputControlOptions | Returns the output control options of the optimization |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
StopCondition | Returns the stop condition to end the optimization |
Tag | Returns the Tag for this object. |
RestrictAreas | Represents the restrict area collection belonging to this optimization solution |
Constraints | Represents the response constrain collection belonging to this optimization solution |
DesignVariables | Represents the design variable collection belonging to this optimization solution |
Smoothings | Represents the smooth collection belonging to this optimization solution |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Destroy | Deletes an optimization solution and the associated result file optional |
Find | Finds the NXOpen.TaggedObject with the given identifier as recorded in a journal. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetIterationNumber | Returns the iteration number during the optimization |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetPostResult | Returns the post result file name and status |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSmoothResult | Returns the result file name and status for a specified smoothing setting |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
Rename | Rename Solution and optionally rename associated results files |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Solve | Solves the optimization solution |
Enumerations¶
TBSOptimizationSolutionResultStatus Enumeration | Define the status of optimization result |
Property Detail¶
ControlParameters¶
-
TBSOptimizationSolution.
ControlParameters
¶ Returns the parameters to control optimization
-------------------------------------
Getter Method
Signature
ControlParameters
Returns: Return type: NXOpen.CAE.Optimization.TBSOptimizationParameters
New in version NX8.0.0.
License requirements: None.
DesignArea¶
-
TBSOptimizationSolution.
DesignArea
¶ Returns the design area that will be modified during optimization
-------------------------------------
Getter Method
Signature
DesignArea
Returns: Return type: NXOpen.CAE.Optimization.TBSDesignArea
New in version NX8.0.0.
License requirements: None.
IsOccurrence¶
-
TBSOptimizationSolution.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
TBSOptimizationSolution.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
TBSOptimizationSolution.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Objectives¶
-
TBSOptimizationSolution.
Objectives
¶ Returns the objective function of the optimization
-------------------------------------
Getter Method
Signature
Objectives
Returns: Return type: NXOpen.CAE.Optimization.TBSObjectives
New in version NX8.0.0.
License requirements: None.
OutputControlOptions¶
-
TBSOptimizationSolution.
OutputControlOptions
¶ Returns the output control options of the optimization
-------------------------------------
Getter Method
Signature
OutputControlOptions
Returns: Return type: NXOpen.CAE.Optimization.TBSOutputControlOptions
New in version NX8.0.0.
License requirements: None.
OwningComponent¶
-
TBSOptimizationSolution.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
TBSOptimizationSolution.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
TBSOptimizationSolution.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
StopCondition¶
-
TBSOptimizationSolution.
StopCondition
¶ Returns the stop condition to end the optimization
-------------------------------------
Getter Method
Signature
StopCondition
Returns: Return type: NXOpen.CAE.Optimization.TBSStopCondition
New in version NX8.0.0.
License requirements: None.
RestrictAreas¶
-
TBSOptimizationSolution.
RestrictAreas
¶ Represents the restrict area collection belonging to this optimization solution
Signature
RestrictAreas
New in version NX8.0.0.
Returns: Return type: NXOpen.CAE.Optimization.TBSRestrictAreaCollection
Constraints¶
-
TBSOptimizationSolution.
Constraints
¶ Represents the response constrain collection belonging to this optimization solution
Signature
Constraints
New in version NX8.0.0.
Returns: Return type: NXOpen.CAE.Optimization.TBSConstraintCollection
DesignVariables¶
-
TBSOptimizationSolution.
DesignVariables
¶ Represents the design variable collection belonging to this optimization solution
Signature
DesignVariables
New in version NX8.0.0.
Returns: Return type: NXOpen.CAE.Optimization.TBSDesignVariableCollection
Smoothings¶
-
TBSOptimizationSolution.
Smoothings
¶ Represents the smooth collection belonging to this optimization solution
Signature
Smoothings
New in version NX8.0.0.
Returns: Return type: NXOpen.CAE.Optimization.TBSSmoothCollection
Method Detail¶
Destroy¶
-
TBSOptimizationSolution.
Destroy
¶ Deletes an optimization solution and the associated result file optional
Signature
Destroy(deleteResult)
Parameters: deleteResult (bool) – true if you want associated result files to be deleted as well New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Find¶
-
TBSOptimizationSolution.
Find
¶ Finds the
NXOpen.TaggedObject
with the given identifier as recorded in a journal.In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with the given journal identifier.
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX8.0.0.
License requirements: None.
FindObject¶
-
TBSOptimizationSolution.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetIterationNumber¶
-
TBSOptimizationSolution.
GetIterationNumber
¶ Returns the iteration number during the optimization
Signature
GetIterationNumber()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
GetPostResult¶
-
TBSOptimizationSolution.
GetPostResult
¶ Returns the post result file name and status
Signature
GetPostResult(iterationID)
Parameters: iterationID (int) – Returns: a tuple Return type: A tuple consisting of (status, postResultName). status is a NXOpen.CAE.Optimization.TBSOptimizationSolutionResultStatus
. postResultName is a str.New in version NX8.0.0.
License requirements: None.
GetSmoothResult¶
-
TBSOptimizationSolution.
GetSmoothResult
¶ Returns the result file name and status for a specified smoothing setting
Signature
GetSmoothResult(smooth)
Parameters: smooth ( NXOpen.CAE.Optimization.TBSSmooth
) –Returns: a tuple Return type: A tuple consisting of (status, smoothResultName). status is a NXOpen.CAE.Optimization.TBSOptimizationSolutionResultStatus
. smoothResultName is a str.New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.CAE.Optimization.TBSSmooth.GetResults()
instead.License requirements: None.
Print¶
-
TBSOptimizationSolution.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
Rename¶
-
TBSOptimizationSolution.
Rename
¶ Rename Solution and optionally rename associated results files
Signature
Rename(name, renameResults)
Parameters: - name (str) – new solution name
- renameResults (bool) – true if you what associated results files to be renamed as well
New in version NX8.0.0.
License requirements: None.
SetName¶
-
TBSOptimizationSolution.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.