TBSOptimizationSolutionResultStatus Enumeration¶
NXOpen.CAE.Optimization.TBSOptimizationSolution.ResultStatus is an alias for NXOpen.CAE.Optimization.TBSOptimizationSolutionResultStatus
-
class
NXOpen.CAE.Optimization.
TBSOptimizationSolutionResultStatus
¶ Bases:
object
Define the status of optimization result
Enum Members
Enum Member Enum Member Description Valid The result is valid OutOfDate The result is out-of-date Invalid The result is invalid -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-