TBSDesignResponseBuilder Class¶
-
class
NXOpen.CAE.Optimization.
TBSDesignResponseBuilder
¶ Bases:
NXOpen.CAE.Optimization.TBSBaseDesignVariableBuilder
Represents the builder of
NXOpen.CAE.Optimization.TBSDesignResponse
To create a new instance of this class, use
NXOpen.CAE.Optimization.TBSOptimizationManager.CreateDesignResponseBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DesignElements | Returns the element group in which the value of the design variable is to be determined |
DesignNodes | Returns the node group in which the value of the design variable is to be determined |
GroupOperatorOption | Returns or sets the group operator option |
LoadCases | Returns the load cases |
NameDescription | Returns the name description |
ReferenceCoordinateSystem | Returns or sets the referenced coordinate system |
SelectionAreaType | Returns or sets the type of selection location on which design variable is applied |
Tag | Returns the Tag for this object. |
VariableType | Returns or sets the varialbe type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TBSDesignResponseBuilderResponse Enumeration | Defines the design response type |
Property Detail¶
VariableType¶
-
TBSDesignResponseBuilder.
VariableType
¶ Returns or sets the varialbe type
-------------------------------------
Getter Method
Signature
VariableType
Returns: Return type: NXOpen.CAE.Optimization.TBSDesignResponseBuilderResponse
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VariableType
Parameters: categoryOption ( NXOpen.CAE.Optimization.TBSDesignResponseBuilderResponse
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Method Detail¶
Validate¶
-
TBSDesignResponseBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.