TBSBaseDesignVariableBuilder Class¶
-
class
NXOpen.CAE.Optimization.
TBSBaseDesignVariableBuilder
¶ Bases:
NXOpen.Builder
Represents the builder of
NXOpen.CAE.Optimization.TBSDesignVariable
This is an abstract class, and cannot be created.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DesignElements | Returns the element group in which the value of the design variable is to be determined |
DesignNodes | Returns the node group in which the value of the design variable is to be determined |
GroupOperatorOption | Returns or sets the group operator option |
LoadCases | Returns the load cases |
NameDescription | Returns the name description |
ReferenceCoordinateSystem | Returns or sets the referenced coordinate system |
SelectionAreaType | Returns or sets the type of selection location on which design variable is applied |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TBSBaseDesignVariableBuilderGroupOperator Enumeration | Defines the operator type to determine the design variable that used within the selection area |
Property Detail¶
DesignElements¶
-
TBSBaseDesignVariableBuilder.
DesignElements
¶ Returns the element group in which the value of the design variable is to be determined
-------------------------------------
Getter Method
Signature
DesignElements
Returns: Return type: NXOpen.CAE.Optimization.TBSGroupDefinition
New in version NX8.0.0.
License requirements: None.
DesignNodes¶
-
TBSBaseDesignVariableBuilder.
DesignNodes
¶ Returns the node group in which the value of the design variable is to be determined
-------------------------------------
Getter Method
Signature
DesignNodes
Returns: Return type: NXOpen.CAE.Optimization.TBSGroupDefinition
New in version NX8.0.0.
License requirements: None.
GroupOperatorOption¶
-
TBSBaseDesignVariableBuilder.
GroupOperatorOption
¶ Returns or sets the group operator option
-------------------------------------
Getter Method
Signature
GroupOperatorOption
Returns: Return type: NXOpen.CAE.Optimization.TBSBaseDesignVariableBuilderGroupOperator
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GroupOperatorOption
Parameters: groupOperatorOption ( NXOpen.CAE.Optimization.TBSBaseDesignVariableBuilderGroupOperator
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
LoadCases¶
-
TBSBaseDesignVariableBuilder.
LoadCases
¶ Returns the load cases
-------------------------------------
Getter Method
Signature
LoadCases
Returns: Return type: NXOpen.CAE.Optimization.TBSLoadCaseManager
New in version NX8.0.0.
License requirements: None.
NameDescription¶
-
TBSBaseDesignVariableBuilder.
NameDescription
¶ Returns the name description
-------------------------------------
Getter Method
Signature
NameDescription
Returns: Return type: NXOpen.CAE.Optimization.NameDescription
New in version NX8.0.0.
License requirements: None.
ReferenceCoordinateSystem¶
-
TBSBaseDesignVariableBuilder.
ReferenceCoordinateSystem
¶ Returns or sets the referenced coordinate system
-------------------------------------
Getter Method
Signature
ReferenceCoordinateSystem
Returns: Return type: NXOpen.CoordinateSystem
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceCoordinateSystem
Parameters: referenceCsys ( NXOpen.CoordinateSystem
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
SelectionAreaType¶
-
TBSBaseDesignVariableBuilder.
SelectionAreaType
¶ Returns or sets the type of selection location on which design variable is applied
-------------------------------------
Getter Method
Signature
SelectionAreaType
Returns: Return type: NXOpen.CAE.Optimization.TBSGroupDefinitionGroupElementType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionAreaType
Parameters: areaType ( NXOpen.CAE.Optimization.TBSGroupDefinitionGroupElementType
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Method Detail¶
Validate¶
-
TBSBaseDesignVariableBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.