TBSShapeLinkConditionManufacturingOption Enumeration¶
NXOpen.CAE.Optimization.TBSShapeLinkCondition.ManufacturingOption is an alias for NXOpen.CAE.Optimization.TBSShapeLinkConditionManufacturingOption
-
class
NXOpen.CAE.Optimization.
TBSShapeLinkConditionManufacturingOption
¶ Bases:
object
Defines the type of link condition
Enum Members
Enum Member Enum Member Description PlaneSymmetry Plane symmetry referring to the plane which lies perpendicular to the given axis of the coordinate system RotationSymmetry Rotation symmetry definition SurfaceStamp Stampable surface definition SurfaceTurn Turnable surface definition SurfaceDrill Drillable surface definition SurfaceDemold Demold surface definition -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-