DAODesignVariableBuilder Class¶
-
class
NXOpen.CAE.Optimization.
DAODesignVariableBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.Optimization.DAODesignVariableBuilder
.To create a new instance of this class, use
NXOpen.CAE.Optimization.DAOSolutionCollection.CreateDesignVariableBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
GlobalSensitivityFlag | Returns or sets the flag if mark current design variable as global sensitivity design variable, only effective for global sensitivity optimization type |
LowerLimit | Returns or sets the lower limit value |
Name | Returns or sets the design variable name |
Tag | Returns the Tag for this object. |
UpperLimit | Returns or sets the upper limit value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetVariable | Gets the design variable |
SetVariable | Sets the design variable |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DAODesignVariableBuilderVariable Enumeration | Represents the design variable type |
Property Detail¶
GlobalSensitivityFlag¶
-
DAODesignVariableBuilder.
GlobalSensitivityFlag
¶ Returns or sets the flag if mark current design variable as global sensitivity design variable, only effective for global sensitivity optimization type
-------------------------------------
Getter Method
Signature
GlobalSensitivityFlag
Returns: Global sensitivity design variable flag Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GlobalSensitivityFlag
Parameters: globalSensitivityFlag (bool) – Global sensitivity design variable flag New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
LowerLimit¶
-
DAODesignVariableBuilder.
LowerLimit
¶ Returns or sets the lower limit value
-------------------------------------
Getter Method
Signature
LowerLimit
Returns: Lower limit value Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerLimit
Parameters: lowerLimit (float) – Lower limit value New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Name¶
-
DAODesignVariableBuilder.
Name
¶ Returns or sets the design variable name
-------------------------------------
Getter Method
Signature
Name
Returns: Design variable name Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: designVariableName (str) – Design variable name New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
UpperLimit¶
-
DAODesignVariableBuilder.
UpperLimit
¶ Returns or sets the upper limit value
-------------------------------------
Getter Method
Signature
UpperLimit
Returns: Upper limit value Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperLimit
Parameters: upperLimit (float) – Upper limit value New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
GetVariable¶
-
DAODesignVariableBuilder.
GetVariable
¶ Gets the design variable
Signature
GetVariable()
Returns: a tuple Return type: A tuple consisting of (variableType, variableExpression). variableType is a NXOpen.CAE.Optimization.DAODesignVariableBuilderVariable
. Variable type variableExpression is aNXOpen.Expression
. Variable expressionNew in version NX8.0.1.
License requirements: None.
SetVariable¶
-
DAODesignVariableBuilder.
SetVariable
¶ Sets the design variable
Signature
SetVariable(variableType, variableExpression)
Parameters: - variableType (
NXOpen.CAE.Optimization.DAODesignVariableBuilderVariable
) – Variable type - variableExpression (
NXOpen.Expression
) – Variable Expression
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- variableType (
Validate¶
-
DAODesignVariableBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.