DAODesignVariableBuilderVariable Enumeration¶
NXOpen.CAE.Optimization.DAODesignVariableBuilder.Variable is an alias for NXOpen.CAE.Optimization.DAODesignVariableBuilderVariable
-
class
NXOpen.CAE.Optimization.
DAODesignVariableBuilderVariable
¶ Bases:
object
Represents the design variable type
Enum Members
Enum Member Enum Member Description SectionProperty Section property variables ShellProperty Shell property variables FeatureDimension Feature dimension variables SketchDimension Sketch dimension variables AllExpressions Variables from FEM, SIM and master part Count Variable type count -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-