TBSCheckDOFDofSettings_Struct Struct

NXOpen.CAE.Optimization.TBSCheckDOF.DofSettings is an alias for NXOpen.CAE.Optimization.TBSCheckDOFDofSettings_Struct

class NXOpen.CAE.Optimization.TBSCheckDOFDofSettings_Struct

Bases: object

the displacement restriction settings on three axial directions of referenced coordinate system .

Constructor: NXOpen.CAE.Optimization.TBSCheckDOF.DofSettings()

Fields

Field Description
Dof1 Represents displacement in the X axial direction
Dof2 Represents displacement in the Y axial direction
Dof3 Represents displacement in the Z axial direction

Dof1

TBSCheckDOFDofSettings_Struct.Dof1

Represents displacement in the X axial direction -------------------------------------

Field Value Type:NXOpen.CAE.Optimization.TBSCheckDOFCheckDofOption

Dof2

TBSCheckDOFDofSettings_Struct.Dof2

Represents displacement in the Y axial direction -------------------------------------

Field Value Type:NXOpen.CAE.Optimization.TBSCheckDOFCheckDofOption

Dof3

TBSCheckDOFDofSettings_Struct.Dof3

Represents displacement in the Z axial direction -------------------------------------

Field Value Type:NXOpen.CAE.Optimization.TBSCheckDOFCheckDofOption