TBSTestFunctionDirection Enumeration¶
NXOpen.CAE.Optimization.TBSTestFunction.Direction is an alias for NXOpen.CAE.Optimization.TBSTestFunctionDirection
-
class
NXOpen.CAE.Optimization.
TBSTestFunctionDirection
¶ Bases:
object
the direction of test displacements
Enum Members
Enum Member Enum Member Description Grow Standard growth Shrink Standard Shrinkage Random Non-standard nodal random displacement -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-