TBSCastConditionMiddlePlaneType Enumeration¶
NXOpen.CAE.Optimization.TBSCastCondition.MiddlePlaneType is an alias for NXOpen.CAE.Optimization.TBSCastConditionMiddlePlaneType
-
class
NXOpen.CAE.Optimization.
TBSCastConditionMiddlePlaneType
¶ Bases:
object
Defines the middle plane type
Enum Members
Enum Member Enum Member Description NotSet No definition of a central plane Automatic Automatica determinaton of the central plane AutomaticTight No holes are generated in the central plane Point A point within the central plane from which the deformation vector is positioned perpendicular to Surface The elements are demolded at the actual surface of the restrict area Stamp The element group is demolded keeping a stampable structure -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-