Goal Enumeration¶
-
class
NXOpen.CAE.Optimization.
Goal
¶ Bases:
object
Represents the goal type Enum Members
Enum Member Enum Member Description Minimum Minimum value Maximum Maximum value Target Target value -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-