DAOSolutionBuilder Class¶
-
class
NXOpen.CAE.Optimization.
DAOSolutionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.Optimization.DAOSolutionBuilder
.To create a new instance of this class, use
NXOpen.CAE.Optimization.DAOSolutionCollection.CreateOptimizationBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AnalysisSolution | Returns or sets the optimization solution analysis solution |
Name | Returns or sets the optimization solution name |
SolverType | Returns or sets the optimization solution solver type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AnalysisSolution¶
-
DAOSolutionBuilder.
AnalysisSolution
¶ Returns or sets the optimization solution analysis solution
-------------------------------------
Getter Method
Signature
AnalysisSolution
Returns: Analysis solution of optimization solution Return type: NXOpen.CAE.SimSolution
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnalysisSolution
Parameters: analysisSolution ( NXOpen.CAE.SimSolution
) – Analysis solution of optimization solutionNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Name¶
-
DAOSolutionBuilder.
Name
¶ Returns or sets the optimization solution name
-------------------------------------
Getter Method
Signature
Name
Returns: Optimization solution name Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: solutionName (str) – Optimization solution name New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SolverType¶
-
DAOSolutionBuilder.
SolverType
¶ Returns or sets the optimization solution solver type
-------------------------------------
Getter Method
Signature
SolverType
Returns: Optimization solution solver type Return type: NXOpen.CAE.Optimization.Solver
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SolverType
Parameters: solverType ( NXOpen.CAE.Optimization.Solver
) – Optimization solution solver typeNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
Validate¶
-
DAOSolutionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.