TBSConstraintBuilderConstraintOption Enumeration¶
NXOpen.CAE.Optimization.TBSConstraintBuilder.ConstraintOption is an alias for NXOpen.CAE.Optimization.TBSConstraintBuilderConstraintOption
-
class
NXOpen.CAE.Optimization.
TBSConstraintBuilderConstraintOption
¶ Bases:
object
Defines the constraint type
Enum Members
Enum Member Enum Member Description Eq Value of equality constraint Lt Value of greater or equal constraint Gt Value of less or equal constraint -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-