DAOSolution Class¶
-
class
NXOpen.CAE.Optimization.
DAOSolution
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.CAE.Optimization.DAOSolution
.To create or edit an instance of this class, use
NXOpen.CAE.Optimization.DAOSolutionBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns or sets the optimization solution name |
OptimizerControl | Returns or sets the optimization solution optimizer control |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
SolverType | Returns or sets the optimization solution solver type |
Tag | Returns the Tag for this object. |
DesignConstraint | Returns the optimization design constraint collection. |
DesignVariable | Returns the optimization design variable collection. |
Methods¶
Method | Description |
---|---|
ActivateSolution | Activates the optimization solution setup |
CreateAttributeIterator | Create an attribute iterator |
CreateConstraintBuilder | Creates the builder object of optimization solution design constraint |
CreateDesignVariableBuilder | Creates the builder object of optimization solution design variable |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteSolution | Deletes the optimization solution |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDesignConstraints | Gets the optimization solution design constraints |
GetDesignObjective | Gets the optimization solution design objective |
GetGlobalSensitivityDesignVariables | Gets the optimization solution design variables for global sensitivity optimization type |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetOptimizationDesignVariables | Gets the optimization solution design variables for general optimization type |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSolutionControls | Gets the optimization solution optimizer control |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDesignConstraints | Sets the optimization solution design constraints |
SetGlobalSensitivityDesignVariables | Sets the optimization solution design variables for global sensitivity optimization type |
SetOptimizationDesignVariables | Sets the optimization solution design variables for general optimization type |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Solve | Solves the optimization solution |
Property Detail¶
IsOccurrence¶
-
DAOSolution.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
DAOSolution.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
DAOSolution.
Name
¶ Returns or sets the optimization solution name
-------------------------------------
Getter Method
Signature
Name
Returns: Solution name Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: solutionName (str) – Solution name New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
OptimizerControl¶
-
DAOSolution.
OptimizerControl
¶ Returns or sets the optimization solution optimizer control
-------------------------------------
Getter Method
Signature
OptimizerControl
Returns: Optimizer control Return type: NXOpen.CAE.Optimization.DAOStopCondition
New in version NX8.0.0.
Deprecated since version NX9.0.0: Not a valid method. Use
NXOpen.CAE.Optimization.DAOSolution.GetSolutionControls()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
OptimizerControl
Parameters: optimizerControl ( NXOpen.CAE.Optimization.DAOStopCondition
) – Optimizer controlNew in version NX8.0.0.
Deprecated since version NX9.0.0: Not a valid method. Use
NXOpen.CAE.Optimization.DAOSolution.GetSolutionControls()
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
OwningComponent¶
-
DAOSolution.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
DAOSolution.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
DAOSolution.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
SolverType¶
-
DAOSolution.
SolverType
¶ Returns or sets the optimization solution solver type
-------------------------------------
Getter Method
Signature
SolverType
Returns: Optimization solution solver type Return type: NXOpen.CAE.Optimization.Solver
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SolverType
Parameters: solverType ( NXOpen.CAE.Optimization.Solver
) – Optimization solution solver typeNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DesignConstraint¶
-
DAOSolution.
DesignConstraint
¶ Returns the optimization design constraint collection.
Signature
DesignConstraint
New in version NX8.0.0.
Returns: Return type: NXOpen.CAE.Optimization.DAOConstraintCollection
DesignVariable¶
-
DAOSolution.
DesignVariable
¶ Returns the optimization design variable collection.
Signature
DesignVariable
New in version NX8.0.0.
Returns: Return type: NXOpen.CAE.Optimization.DAODesignVariableCollection
Method Detail¶
ActivateSolution¶
-
DAOSolution.
ActivateSolution
¶ Activates the optimization solution setup
Signature
ActivateSolution()
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateConstraintBuilder¶
-
DAOSolution.
CreateConstraintBuilder
¶ Creates the builder object of optimization solution design constraint
Signature
CreateConstraintBuilder(optimizationConstraint)
Parameters: optimizationConstraint ( NXOpen.CAE.Optimization.DAOConstraint
) – Design constraintReturns: Design constraint builder Return type: NXOpen.CAE.Optimization.DAOConstraintBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateDesignVariableBuilder¶
-
DAOSolution.
CreateDesignVariableBuilder
¶ Creates the builder object of optimization solution design variable
Signature
CreateDesignVariableBuilder(optimizationDesvar)
Parameters: optimizationDesvar ( NXOpen.CAE.Optimization.DAODesignVariable
) – Design variableReturns: Design variable builder Return type: NXOpen.CAE.Optimization.DAODesignVariableBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteSolution¶
-
DAOSolution.
DeleteSolution
¶ Deletes the optimization solution
Signature
DeleteSolution()
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
DAOSolution.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetDesignConstraints¶
-
DAOSolution.
GetDesignConstraints
¶ Gets the optimization solution design constraints
Signature
GetDesignConstraints()
Returns: Design constraints Return type: list of NXOpen.CAE.Optimization.DAOConstraint
New in version NX8.0.0.
License requirements: None.
GetDesignObjective¶
-
DAOSolution.
GetDesignObjective
¶ Gets the optimization solution design objective
Signature
GetDesignObjective()
Returns: Design objective Return type: NXOpen.CAE.Optimization.DAOObjective
New in version NX8.0.0.
License requirements: None.
GetGlobalSensitivityDesignVariables¶
-
DAOSolution.
GetGlobalSensitivityDesignVariables
¶ Gets the optimization solution design variables for global sensitivity optimization type
Signature
GetGlobalSensitivityDesignVariables()
Returns: Design variables Return type: list of NXOpen.CAE.Optimization.DAODesignVariable
New in version NX8.0.0.
License requirements: None.
GetOptimizationDesignVariables¶
-
DAOSolution.
GetOptimizationDesignVariables
¶ Gets the optimization solution design variables for general optimization type
Signature
GetOptimizationDesignVariables()
Returns: Design variables Return type: list of NXOpen.CAE.Optimization.DAODesignVariable
New in version NX8.0.0.
License requirements: None.
GetSolutionControls¶
-
DAOSolution.
GetSolutionControls
¶ Gets the optimization solution optimizer control
Signature
GetSolutionControls()
Returns: Optimizer control Return type: NXOpen.CAE.Optimization.DAOStopCondition
New in version NX9.0.0.
License requirements: None.
Print¶
-
DAOSolution.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetDesignConstraints¶
-
DAOSolution.
SetDesignConstraints
¶ Sets the optimization solution design constraints
Signature
SetDesignConstraints(designConstraints)
Parameters: designConstraints (list of NXOpen.CAE.Optimization.DAOConstraint
) – Design constraintsNew in version NX8.0.0.
Deprecated since version NX9.0.0: Not a valid method. Use
NXOpen.CAE.Optimization.DAOSolution.CreateConstraintBuilder()
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetGlobalSensitivityDesignVariables¶
-
DAOSolution.
SetGlobalSensitivityDesignVariables
¶ Sets the optimization solution design variables for global sensitivity optimization type
Signature
SetGlobalSensitivityDesignVariables(designVariables)
Parameters: designVariables (list of NXOpen.CAE.Optimization.DAODesignVariable
) – Design variablesNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetOptimizationDesignVariables¶
-
DAOSolution.
SetOptimizationDesignVariables
¶ Sets the optimization solution design variables for general optimization type
Signature
SetOptimizationDesignVariables(designVariables)
Parameters: designVariables (list of NXOpen.CAE.Optimization.DAOConstraint
) – Design variablesNew in version NX8.0.0.
Deprecated since version NX9.0.0: Not a valid method. Use
NXOpen.CAE.Optimization.DAOSolution.CreateDesignVariableBuilder()
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)