TBSShapeOptimizationParameters Class¶
-
class
NXOpen.CAE.Optimization.
TBSShapeOptimizationParameters
¶ Bases:
NXOpen.CAE.Optimization.TBSOptimizationParameters
Represents the control parameters of shape optimization
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
DisplacementStepSize | Returns or sets the step size option for modifying the displacement during the optimization operation |
Scale | Returns or sets the scale factor |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
TBSShapeOptimizationParametersDisplacementStepsize Enumeration | the step size option for incrementing the displacement during the optimization operation |
Property Detail¶
DisplacementStepSize¶
-
TBSShapeOptimizationParameters.
DisplacementStepSize
¶ Returns or sets the step size option for modifying the displacement during the optimization operation
-------------------------------------
Getter Method
Signature
DisplacementStepSize
Returns: Return type: NXOpen.CAE.Optimization.TBSShapeOptimizationParametersDisplacementStepsize
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplacementStepSize
Parameters: stepSizeOption ( NXOpen.CAE.Optimization.TBSShapeOptimizationParametersDisplacementStepsize
) –New in version NX8.5.0.
License requirements: cae_opt_toposhape (“NX Shape Optimization”)
Scale¶
-
TBSShapeOptimizationParameters.
Scale
¶ Returns or sets the scale factor
-------------------------------------
Getter Method
Signature
Scale
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Scale
Parameters: scale (float) – New in version NX8.5.0.
License requirements: cae_opt_toposhape (“NX Shape Optimization”)