TBSLoadCase Class¶
-
class
NXOpen.CAE.Optimization.
TBSLoadCase
¶ Bases:
NXOpen.TaggedObject
Represents the load case
To create a new instance of this class, use
NXOpen.CAE.Optimization.TBSOptimizationManager.CreateLoadCase()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ShellLayer | Returns or sets the shell layer |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetSubcase | Returns the load cases |
GetSubstep | Returns the substeps |
SetSubcase | Sets the load cases |
SetSubstep | Sets the sub steps |
Enumerations¶
TBSLoadCaseLayerOption Enumeration | Defines the location for calcuating shell stresses |
Property Detail¶
ShellLayer¶
-
TBSLoadCase.
ShellLayer
¶ Returns or sets the shell layer
-------------------------------------
Getter Method
Signature
ShellLayer
Returns: Return type: NXOpen.CAE.Optimization.TBSLoadCaseLayerOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShellLayer
Parameters: layer ( NXOpen.CAE.Optimization.TBSLoadCaseLayerOption
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Method Detail¶
GetSubcase¶
-
TBSLoadCase.
GetSubcase
¶ Returns the load cases
Signature
GetSubcase()
Returns: a tuple Return type: A tuple consisting of (allSubcase, subcaseId) allSubcase is a bool. subcaseId is a int. New in version NX8.0.0.
License requirements: None.
GetSubstep¶
-
TBSLoadCase.
GetSubstep
¶ Returns the substeps
Signature
GetSubstep()
Returns: a tuple Return type: A tuple consisting of (allSubSteps, subSteps) allSubSteps is a bool. subSteps is a list of int. New in version NX8.0.0.
License requirements: None.
SetSubcase¶
-
TBSLoadCase.
SetSubcase
¶ Sets the load cases
Signature
SetSubcase(allSubcases, subcaseId)
Parameters: - allSubcases (bool) –
- subcaseId (int) –
New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
SetSubstep¶
-
TBSLoadCase.
SetSubstep
¶ Sets the sub steps
Signature
SetSubstep(allSubSteps, subSteps)
Parameters: - allSubSteps (bool) –
- subSteps (list of int) –
New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)