TBSTopologyControllerOptimizationParameters Class¶
-
class
NXOpen.CAE.Optimization.
TBSTopologyControllerOptimizationParameters
¶ Bases:
NXOpen.CAE.Optimization.TBSOptimizationParameters
Represents the parameters to control an optimization in controller strategy
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AutomaticFrozenOption | Returns or sets the automatic frozen option |
IterationNumbers | Returns or sets the number of iterations. |
SpeedOption | Returns or sets the speed size of increment |
StartDeleteVolume | Returns or sets the volume that is deleted in the first design cycle |
Tag | Returns the Tag for this object. |
VolumeDefinitionOption | Returns or sets the volume definition option |
Methods¶
Enumerations¶
TBSTopologyControllerOptimizationParametersAutoFrozen Enumeration | Defines the automatic fromzen strategy |
TBSTopologyControllerOptimizationParametersSpeed Enumeration | Specifies the step size of increment |
TBSTopologyControllerOptimizationParametersVolumeDefinitionMethod Enumeration | Represents the definition of volume that can be removed immediatedly in the first design cycle |
Property Detail¶
AutomaticFrozenOption¶
-
TBSTopologyControllerOptimizationParameters.
AutomaticFrozenOption
¶ Returns or sets the automatic frozen option
-------------------------------------
Getter Method
Signature
AutomaticFrozenOption
Returns: Return type: NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParametersAutoFrozen
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutomaticFrozenOption
Parameters: autoFrozen ( NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParametersAutoFrozen
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
IterationNumbers¶
-
TBSTopologyControllerOptimizationParameters.
IterationNumbers
¶ Returns or sets the number of iterations.
Only available when
CAE.Optimization.TBSTopologyControllerOptimizationParameters.SpeedOption()
isCAE.Optimization.TBSTopologyControllerOptimizationParametersSpeed.Iteration
-------------------------------------
Getter Method
Signature
IterationNumbers
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterationNumbers
Parameters: numIterations (int) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
SpeedOption¶
-
TBSTopologyControllerOptimizationParameters.
SpeedOption
¶ Returns or sets the speed size of increment
-------------------------------------
Getter Method
Signature
SpeedOption
Returns: Return type: NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParametersSpeed
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpeedOption
Parameters: speedOption ( NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParametersSpeed
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
StartDeleteVolume¶
-
TBSTopologyControllerOptimizationParameters.
StartDeleteVolume
¶ Returns or sets the volume that is deleted in the first design cycle
-------------------------------------
Getter Method
Signature
StartDeleteVolume
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartDeleteVolume
Parameters: startDeleteVolume (float) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
VolumeDefinitionOption¶
-
TBSTopologyControllerOptimizationParameters.
VolumeDefinitionOption
¶ Returns or sets the volume definition option
-------------------------------------
Getter Method
Signature
VolumeDefinitionOption
Returns: Return type: NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParametersVolumeDefinitionMethod
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VolumeDefinitionOption
Parameters: volumeDefinitionOption ( NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParametersVolumeDefinitionMethod
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)