TBSTopologySensitivityOptimizationParametersDensityUpdate Enumeration¶
NXOpen.CAE.Optimization.TBSTopologySensitivityOptimizationParameters.DensityUpdate is an alias for NXOpen.CAE.Optimization.TBSTopologySensitivityOptimizationParametersDensityUpdate
-
class
NXOpen.CAE.Optimization.
TBSTopologySensitivityOptimizationParametersDensityUpdate
¶ Bases:
object
the method defines how the densities are updated in the method of moving asymptotes
Enum Members
Enum Member Enum Member Description Normal Normal strategy Conservative Conservative strategy Agressive Agressive strategy -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-