TBSEigenvalueOptimizationParameters Class¶
-
class
NXOpen.CAE.Optimization.
TBSEigenvalueOptimizationParameters
¶ Bases:
NXOpen.TaggedObject
Represents the parameters to control an eigenvalue optimization
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ModeNumber | Returns or sets the number of modes included in the mode tracking |
Tag | Returns the Tag for this object. |
TrackingMode | Returns or sets the switch for mode tracking |
TrackingNodes | Returns the tracking nodes, only available when CAE.Optimization.TBSEigenvalueOptimizationParameters.TrackingMode`() is True |
Methods¶
Property Detail¶
ModeNumber¶
-
TBSEigenvalueOptimizationParameters.
ModeNumber
¶ Returns or sets the number of modes included in the mode tracking
-------------------------------------
Getter Method
Signature
ModeNumber
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModeNumber
Parameters: modeNumber (int) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
TrackingMode¶
-
TBSEigenvalueOptimizationParameters.
TrackingMode
¶ Returns or sets the switch for mode tracking
-------------------------------------
Getter Method
Signature
TrackingMode
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrackingMode
Parameters: trackingMode (bool) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
TrackingNodes¶
-
TBSEigenvalueOptimizationParameters.
TrackingNodes
¶ Returns the tracking nodes, only available when
CAE.Optimization.TBSEigenvalueOptimizationParameters.TrackingMode`()
is True-------------------------------------
Getter Method
Signature
TrackingNodes
Returns: Return type: NXOpen.CAE.Optimization.TBSGroupDefinition
New in version NX8.0.0.
License requirements: None.