TBSTopologySensitivityOptimizationParametersMaterialInterpolation Enumeration¶
NXOpen.CAE.Optimization.TBSTopologySensitivityOptimizationParameters.MaterialInterpolation is an alias for NXOpen.CAE.Optimization.TBSTopologySensitivityOptimizationParametersMaterialInterpolation
-
class
NXOpen.CAE.Optimization.
TBSTopologySensitivityOptimizationParametersMaterialInterpolation
¶ Bases:
object
the relationshp between relative density and relative element stiffness
Enum Members
Enum Member Enum Member Description Simp Solid Isotropic material with penalization Ramp Rational approximation of material properties -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-