NXOpen.Assemblies Package¶
Classes¶
AbsolutePositionBuilder Class | Represents a builder class that absolutely positions the specified objects. |
Arrangement Class | Manages the suppression of NXOpen.Assemblies.Component`s within a :py:class:`NXOpen.Assemblies.ComponentAssembly . |
ArrangementCollection Class | a collection of arrangements |
ArrangementsBuilder Class | Represents an arrangements builder that selects an arrangement |
AssembliesGeneralPropertiesBuilder Class | Represents an NXOpen.Assemblies.AssembliesGeneralPropertiesBuilder to be used for changing the general properties of a component. |
AssembliesParameterPropertiesBuilder Class | Represents an NXOpen.Assemblies.AssembliesParameterPropertiesBuilder to be used for changing the name or modifying the positioning mixture status of a component. |
Assembly Class | Assembly class |
AssemblyManager Class | Represents the Assembly Manager |
AttributeSearchTerm Class | An attribute search term within a NXOpen.Assemblies.SubsetRecipe . |
AttributeSearchTermBuilder Class | An AttributeSearchTermBuilder is used to create or edit an NXOpen.Assemblies.AttributeSearchTerm . |
BoxSearchTerm Class | A volume search term within a NXOpen.Assemblies.SubsetRecipe . |
BoxSearchTermBuilder Class | A BoxSearchTermBuilder is used to create or edit an NXOpen.Assemblies.BoxSearchTerm . |
ClearanceAnalysisBuilder Class | Represents NXOpen.Assemblies.ClearanceAnalysisBuilder . |
ClearanceSet Class | Represents NXOpen.Assemblies.ClearanceSet . |
ClearanceSetCollection Class | Represents NXOpen.Assemblies.ClearanceSetCollection . |
Component Class | Represents a component in a NXOpen.Assemblies.ComponentAssembly . |
ComponentAssembly Class | Represents the set of :py:class:`NXOpen.Assemblies.Component`s that make up an assembly. |
ComponentGroup Class | Represents a Component Group that is defined within an Assembly. |
ComponentGroupCollection Class |
|
ComponentOrder Class | Represents an order object that stores the order of child NXOpen.Assemblies.Component`s in context of parent :py:class:`NXOpen.Assemblies.ComponentAssembly . |
ComponentPattern Class | Represents the component pattern class. |
ComponentPatternBuilder Class | Represents a builder class that performs various NXOpen.Assemblies.ComponentPattern operations. |
ComponentPatternCollection Class | Represents the collection object for all component patterns. |
ConstraintDisplayBuilder Class | The NXOpen.Assemblies.ConstraintDisplayBuilder can be used to control visibility of constraints and optionally components. |
CreateNewComponentBuilder Class | Represents a NXOpen.Assemblies.CreateNewComponentBuilder builder class. |
CreateOverridePartBuilder Class | Represents a builder class that creates empty override part in the specified design elements. |
DeleteOverridePartBuilder Class | Represents a builder class that deletes override part in the specified design elements. |
DesignElementBuilder Class | Represents a builder class that performs various design element operations. |
ExplicitSearchTerm Class | A NXOpen.Assemblies.SubsetRecipe search term that refers explicitly to a design element. |
ExplodedComponent Class | Represents a NXOpen.Assemblies.Component within an explosion. |
Explosion Class | Represents an explosion. |
ExplosionCollection Class | Represents a collection of explosions |
FindInCollaborativeDesign Class | FindInCollaborativeDesign is a searcher for performing simple searches in the context of a subset. |
GroupSearchTerm Class | A group of NXOpen.Assemblies.SearchTerm`s within a :py:class:`NXOpen.Assemblies.SubsetRecipe . |
HideComponentBuilder Class | Represents a NXOpen.Assemblies.HideComponentBuilder |
LoadInterpartDataBuilder Class | Represents a builder:py:class:NXOpen.Assemblies.LoadInterpartDataBuilder |
MakeUniquePartBuilder Class | Represents a NXOpen.Assemblies.MakeUniquePartBuilder builder. |
MechanicalRoutingSubsetBuilder Class | A MechanicalRoutingSubsetBuilder is used to create/edit Subsets NXOpen.Assemblies.Subset that are used to define the context needed to perform a Mechanical Routing Design activity. |
Order Class | Represents base class for all Order classes. |
OrderCollection Class | a collection of :py:class:`NXOpen.Assemblies.Order`s |
Partition Class | A partition is a Teamcenter object in a Collaborative Design. |
PartitionList Class | Represents a list of objects. |
PartitionScheme Class | A partition scheme is a Teamcenter object in a Collaborative Design. |
PartitionSearchTerm Class | A Assemblies.SubsetRecipe search term that refers to a partition. |
PatternInstance Class | Represents the pattern instance object. |
PatternMaster Class | Represents the pattern master object. |
PatternMember Class | Represents the pattern member object. |
PlaneSearchTerm Class | A plane search term within a NXOpen.Assemblies.SubsetRecipe . |
PlaneSearchTermBuilder Class | A PlaneSearchTermBuilder is used to create or edit an NXOpen.Assemblies.PlaneSearchTerm . |
PositioningGroup Class | Represents the class for positioning group. |
PositioningGroupBuilder Class | Represents builder class for positioning group which is used to store constraints for design element. |
PositioningTask Class | Represents the class for positioning task. |
PositioningTaskBuilder Class | Represents the class for positioning task builder |
ProductOutlineBuilder Class | Represents a builder NXOpen.Assemblies.ProductOutlineBuilder . |
ProductOutlineManager Class | Represents a collection of assemblies. |
ProximitySearchTerm Class | A proximity search term within a NXOpen.Assemblies.SubsetRecipe . |
ProximitySearchTermBuilder Class | A ProximitySearchTermBuilder is used to create or edit an Assemblies.BoxSearchTerm . |
RelinkerBuilder Class | Represents a NXOpen.Assemblies.RelinkerBuilder |
RelinkerCollection Class | Represents a collection of relinker |
ReplaceComponentBuilder Class | Represents a NXOpen.Assemblies.ReplaceComponentBuilder builder. |
RunContentProximitySearchTerm Class | A proximity search term within a NXOpen.Assemblies.SubsetRecipe . |
RunContentProximitySearchTermBuilder Class | A RunContentProximitySearchTermBuilder is used to create or edit an Assemblies.RunContentProximitySearchTerm . |
SearchResultCollection Class | A collection of :py:class:`NXOpen.Assemblies.SearchResultElement`s. |
SearchResultElement Class | A search result element can be produced as the result of a search performed in the context of a NXOpen.Assemblies.SubsetBuilder . |
SearchTerm Class | A search term is used to specify a search for the contents of a NXOpen.Assemblies.Subset . |
SearchTermBuilder Class | A SearchTermBuilder is used to create or edit an NXOpen.Assemblies.SearchTerm . |
SelectComponent Class | Represents a single object selection. |
SelectComponentList Class | Represents a list of objects on a selection list. |
ShowComponentBuilder Class | Represents a NXOpen.Assemblies.ShowComponentBuilder |
Subset Class | A subset is a set of design elements within a collaborative design. |
SubsetBuilder Class | A SubsetBuilder is used to create or edit an NXOpen.Assemblies.Subset . |
SubsetCollection Class | Represents a collection of subset. |
SubsetConfigurationBuilder Class | A SubsetConfigurationBuilder is used to edit the revision rule and effectivity used to configure the contents of the subset. |
SubsetRecipe Class | A subset recipe is used by a NXOpen.Assemblies.SubsetBuilder to collect :py:class:`NXOpen.Assemblies.SearchTerm`s. |
UpdateDesignElementPositionBuilder Class | Represents the builder class that updates positions of the DE’s(Shape/Reuse) or Subordinates with override that are out of date. |
UpdateStructureBuilder Class | Represents a builder NXOpen.Assemblies.UpdateStructureBuilder . |
WaveQuery Class | Provides information about the inter-part relations (e.g. WAVE, inter-part expressions) in a NX model. |
Enumerations¶
AssembliesChildRevisionOptions Enumeration | Child revision options |
AssembliesEventTypes Enumeration | NX Event types |
AssembliesGeneralPropertiesBuilderHiddenOptions Enumeration | Options for managing the hidden property on the components |
AssembliesGeneralPropertiesBuilderLayerOptions Enumeration | Layer options for the components |
AssembliesGeneralPropertiesBuilderQuantityOptions Enumeration | Options for assigning the quantity on the components |
AssembliesGeneralPropertiesBuilderReferenceComponentOptions Enumeration | Options for setting the reference-only property on the components |
AssembliesParameterPropertiesBuilderArrangementOptions Enumeration | The positioning mixture status options |
BoxSearchTermBoxOverlapLogicType Enumeration | Logic used to determine the type of inclusion used in a box search term within a recipe. |
ClearanceAnalysisBuilderCalculationMethodType Enumeration | Specify the analysis method. |
ClearanceAnalysisBuilderClearanceBetweenEntity Enumeration | Specify the type of clearance analysis. |
ClearanceAnalysisBuilderClearanceZoneSource Enumeration | Specify the source of the clearance zone |
ClearanceAnalysisBuilderCollectionRange Enumeration | Specify how to compare objects inside a collection. |
ClearanceAnalysisBuilderNumberOfCollections Enumeration | Specify the number of collections used for clearance analysis. |
ClearanceAnalysisBuilderPairExcludedReason Enumeration | Specify the reason for excluding the pair |
ClearanceAnalysisBuilderZoneType Enumeration | Specify the clearance zone type. |
ClearanceSetCopyMode Enumeration | Specify the dataset copy mode |
ClearanceSetInterferenceType Enumeration | Specify the type of interference |
ClearanceSetJobStatus Enumeration | Specify the job aborted status |
ClearanceSetPenetrationDepthResult Enumeration | The result of penetration depth calculation |
ClearanceSetReanalyzeOutOfDateExcludedPairs Enumeration | Specify whether to reanalyze out-of-date excluded pairs. |
ClearanceSetReanalyzePairCalculationMethod Enumeration | The analysis method to use when reanalyzing a pair. |
CollaborativeContentType Enumeration | Represents the collaborative content type corresponding to this component |
ComponentRepresentationMode Enumeration | Representation status of a component |
ComponentAssemblyCheckinCheckoutOption Enumeration | Check in and Check out options for components |
ComponentAssemblyCloseModified Enumeration | Indicates how close component should handle component parts when they are modified |
ComponentAssemblyOpenComponentStatus Enumeration | Open Component Status |
ComponentAssemblyOpenOption Enumeration | Open options for open_components |
ComponentAssemblyOrderTargetLocation Enumeration | Option controls whether reordered NXOpen.Assemblies.Component`s are placed before or after the target :py:class:`NXOpen.Assemblies.Component |
ComponentAssemblySubstitutionMode Enumeration | Defines how a component substitution operation is performed. |
ComponentAssemblySuppressedState Enumeration | Defines the component supression states. |
ComponentQuantity Enumeration | Represents the component quantity type of the component |
ConstraintDisplayBuilderVisibleConstraintsRuleOptions Enumeration | This enum is used to control which constraints are treated as connected to the selected components. |
CreateNewComponentBuilderComponentCamType Enumeration | Set the origin type |
CreateNewComponentBuilderComponentLayerOptionType Enumeration | Set the layer option type |
CreateNewComponentBuilderComponentOriginType Enumeration | Set the cam component type |
CreateNewComponentBuilderComponentReferenceSetType Enumeration | Set the reference set |
DegreesOfFreedomResult Enumeration | The overall result of the degrees of freedom calculation reported in NXOpen.Assemblies.DegreesOfFreedom . |
DegreesOfFreedomStatus Enumeration | The status of a rotation point, rotation axis or translation direction reported in NXOpen.Assemblies.DegreesOfFreedom . |
DesignElementBuilderEditActionType Enumeration | Represents the edit action on a design element |
DesignElementBuilderLayerOptionType Enumeration | Represents the layer option of a design element |
DesignElementBuilderOperationType Enumeration | Represents an operation type that can be performed on a design element |
DesignElementBuilderPositioningOption Enumeration | Represents the positioning option of a design element. |
DesignElementBuilderReferenceSetType Enumeration | Represents the reference set of a design element |
DesignElementBuilderSaveAsActionType Enumeration | Represents the save as action on a design element |
DesignElementBuilderStateType Enumeration | Represents the state of a design element |
FindInCollaborativeDesignObjectType Enumeration | The type of object for which the search is performed. |
FindInCollaborativeDesignSearchType Enumeration | The attribute against which the search text is matched. |
LoadInterpartDataBuilderOpenUnloadedParentsType Enumeration | Represents the load interpart parent level types |
LoadInterpartDataBuilderSelectionScopeType Enumeration | Represents the load interpart selection scope types |
MakeUniquePartBuilderOption Enumeration | Represents possible copy assembly options for unique part |
MechanicalRoutingSubsetBuilderSurroundingDataRecipeMethod Enumeration | Represents the method to use to determine the surrounding data corresponding to the routing design content that has been loaded. |
OrderState Enumeration | Represents whether an order is saved or not |
OrderType Enumeration | Represents the type of an order |
PlaneSearchTermPlaneOverlapLogicType Enumeration | Logic used to determine the type of inclusion used in a plane search term within a recipe. |
PositionOverrideType Enumeration | Represents the type of the positioning override on the component |
PositioningGroupStatus Enumeration | Represents the position status of positioning group |
ProductOutlineBuilderLineFont Enumeration | Represents the line font types |
RelinkerBuilderLinkCategory Enumeration | Represents the link category of Relinker, either geometry WAVE link or interpart expression. |
RelinkerBuilderLinkOption Enumeration | Represents the relink option. |
RelinkerBuilderLinkScope Enumeration | Represents the relink scope type of Relinker. |
RelinkerBuilderLinkType Enumeration | Represents the link type option when browsing current available links. |
ReplaceComponentBuilderComponentLayerOption Enumeration | Represents possible layer option for replacement part |
ReplaceComponentBuilderComponentNameOption Enumeration | Represents possible component name option for replace operation |
ReplaceComponentBuilderComponentReferenceSet Enumeration | Represents possible reference set for replacement part |
SearchTermSearchTermLogicType Enumeration | Logic used to determine how a search term is used within a recipe. |
SubsetContentType Enumeration | Represents the content type for a subset. |
SubsetPartitionViewStyleType Enumeration | Represents the type of partition view style to show for a subset. |
Structs¶
ClearanceSetSummary_Struct Struct | Summary of the most recent Clearance Analysis results |
DegreesOfFreedom Struct | Structure used to report the Degrees of Freedom of a component. |