FindInCollaborativeDesignSearchType Enumeration¶
NXOpen.Assemblies.FindInCollaborativeDesign.SearchType is an alias for NXOpen.Assemblies.FindInCollaborativeDesignSearchType
-
class
NXOpen.Assemblies.
FindInCollaborativeDesignSearchType
¶ Bases:
object
The attribute against which the search text is matched.
Enum Members
Enum Member Enum Member Description ItemQuery Match text with item name or id-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-