ComponentAssemblyOrderTargetLocation Enumeration¶
NXOpen.Assemblies.ComponentAssembly.OrderTargetLocation is an alias for NXOpen.Assemblies.ComponentAssemblyOrderTargetLocation
-
class
NXOpen.Assemblies.
ComponentAssemblyOrderTargetLocation
¶ Bases:
object
Option controls whether reordered
NXOpen.Assemblies.Component`s are placed before or after the target :py:class:`NXOpen.Assemblies.Component
Enum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “PlaceBefore”, ” Move reordered
NXOpen.Assemblies.Component`s before the target :py:class:`NXOpen.Assemblies.Component
” “PlaceAfter”, ” Move reorderedNXOpen.Assemblies.Component`s after the target :py:class:`NXOpen.Assemblies.Component
“
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.