OrderType Enumeration¶
NXOpen.Assemblies.Order.Type is an alias for NXOpen.Assemblies.OrderType
-
class
NXOpen.Assemblies.
OrderType
¶ Bases:
object
Represents the type of an order
Enum Members
Enum Member Enum Member Description UserDefinedComponent User defined component orderSequentialComponent System defined sequential component orderChronologicalComponent System defined chronological component orderAlphanumericComponent System defined alphanumeric component orderAlphabeticComponent System defined alphabetic component order-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-