RelinkerBuilderLinkOption Enumeration¶
NXOpen.Assemblies.RelinkerBuilder.LinkOption is an alias for NXOpen.Assemblies.RelinkerBuilderLinkOption
-
class
NXOpen.Assemblies.
RelinkerBuilderLinkOption
¶ Bases:
object
Represents the relink option.
Per this option, relinker will search the corresponding source and do relinking.
Enum Members
Enum Member Enum Member Description InterpartExpression Indicate relink option is interpart expression onlyWaveGeometry Indicate relink option is wave geometry onlyBoth Indicate relink option is both interpart expression and wave link-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-