ComponentRepresentationMode Enumeration¶
NXOpen.Assemblies.Component.RepresentationMode is an alias for NXOpen.Assemblies.ComponentRepresentationMode
-
class
NXOpen.Assemblies.
ComponentRepresentationMode
¶ Bases:
object
Representation status of a component
Enum Members
Enum Member Enum Member Description Lightweight The component’s solid bodies are all displayed using the lightweight representationPartial The component’s solid bodies are displayed with some being exact and some being shown lightweightExact The component’s solid bodies are displayed with the exact dataNotSet There are no bodies to display for the current component-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-