BoxSearchTermBoxOverlapLogicType Enumeration¶
NXOpen.Assemblies.BoxSearchTerm.BoxOverlapLogicType is an alias for NXOpen.Assemblies.BoxSearchTermBoxOverlapLogicType
-
class
NXOpen.Assemblies.
BoxSearchTermBoxOverlapLogicType
¶ Bases:
object
Logic used to determine the type of inclusion used in a box search term within a recipe.
Enum Members
Enum Member Enum Member Description Inside Include objects residing inside the box defined by this search termOutside Include objects residing outside the box defined by this search termIntersects Include objects that intersect the box defined by this search termInsideOrIntersects Include objects residing inside or intersecting the box defined by this search termOutsideOrIntersects Include objects residing outside or intersecting the box defined by this search term-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-