AssembliesParameterPropertiesBuilderArrangementOptions Enumeration¶
NXOpen.Assemblies.AssembliesParameterPropertiesBuilder.ArrangementOptions is an alias for NXOpen.Assemblies.AssembliesParameterPropertiesBuilderArrangementOptions
-
class
NXOpen.Assemblies.
AssembliesParameterPropertiesBuilderArrangementOptions
¶ Bases:
object
The positioning mixture status options
Enum Members
Enum Member Enum Member Description IndividuallyPositioned All components are variedSamePositionInAll All components are unvariedMixed All components are neither varied nor unvaried-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-