RelinkerBuilderLinkType Enumeration¶
NXOpen.Assemblies.RelinkerBuilder.LinkType is an alias for NXOpen.Assemblies.RelinkerBuilderLinkType
-
class
NXOpen.Assemblies.
RelinkerBuilderLinkType
¶ Bases:
object
Represents the link type option when browsing current available links.
As a filter, it tells Link Browser what links should be listed.
Enum Members
Enum Member Enum Member Description All Indicate relink browser type is allNotBroken Indicate relink browser type is not broken onlyBroken Indicate relink browser type is broken onlyAutoLinked Indicate relink browser type is auto-linked onlyWithMultipleSource Indicate relink browser type is with multuple source-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-