ComponentAssemblyOpenOption Enumeration¶
NXOpen.Assemblies.ComponentAssembly.OpenOption is an alias for NXOpen.Assemblies.ComponentAssemblyOpenOption
-
class
NXOpen.Assemblies.
ComponentAssemblyOpenOption
¶ Bases:
object
Open options for open_components
Enum Members
Enum Member Enum Member Description ComponentOnly Open the component but none of its childrenImmediateChildren Open the immediate children of an already open componentWholeAssembly Open the component and all of its childrenReapplyRevRule Reconfigure and open components based on current revision rules. If this option is used in native mode, it will behave just like Open Component.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-