MechanicalRoutingSubsetBuilder Class¶
-
class
NXOpen.Assemblies.
MechanicalRoutingSubsetBuilder
¶ Bases:
NXOpen.Builder
A MechanicalRoutingSubsetBuilder is used to create/edit Subsets
NXOpen.Assemblies.Subset
that are used to define the context needed to perform a Mechanical Routing Design activity.The builder may generate multiple subsets. The content of these subsets can be classified into “Work” content - the elements of the Routing design that the user would like to focus on and “Surrounding Data” content - the 3D content that surrounds the Routing design. The subset definition process utilizes the concept of a Run ja class TBD by NX P and ID while defining the recipe terms needed for the subsets. To create a new instance of this class, use
NXOpen.Assemblies.SubsetCollection.CreateMechanicalRoutingSubsetBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Fixtures | Returns or sets an option for inclusion of fixtures DE’s in the Routing Work. |
Insulation | Returns or sets an option for inclusion of insulation DE’s in the Routing Work Subset. |
SurroundingDataProximityDistance | Returns or sets a proximity to Routing Content method has been selected to determine the surrounding content then this is the distance value used to perform the evaluation. |
SurroundingDataRecipeMethodType | Returns or sets the routing recipes Assemblies.MechanicalRoutingSubsetBuilder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AppendSearchResultElementToSelectedList | Appends the Search Result Element corresponding to the given Run ID to the SelectedSearchResultElement list on NXOpen.Assemblies.MechanicalRoutingSubsetBuilder . |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetConfigurationContextBuilder | Returns the configuration context builder which will be used by user to set revision rule or effectivity and then user needs to use NXOpen.Assemblies.FindInCollaborativeDesign to search for runs using object type RunElement. |
GetObject | Returns the object currently being edited by this builder. |
GetSearchSubsetBuilder | The subset builder which is used for searching runs, the user will have to use NXOpen.Assemblies.FindInCollaborativeDesign to search for runs using object type RunElement. |
RemoveAllSearchResultElementsFromSelectedList | Removes all the Search Result Element from the SelectedSearchResultElement list on NXOpen.Assemblies.MechanicalRoutingSubsetBuilder . |
RemoveSearchResultElementFromSelectedList | Removes the Search Result Element corresponding to the given Run ID from the SelectedSearchResultElement list on NXOpen.Assemblies.MechanicalRoutingSubsetBuilder . |
SetRoutingSubsetAsWorkPart | The builder may generate multiple subsets. |
SetSearchSubsetBuilder | Sets the subset builder which needs to be set by user to search runs, the user will have to use NXOpen.Assemblies.FindInCollaborativeDesign to search for runs using object type RunElement. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateSubsetUsingConfigurationContext | The routing subsets will be updated (e. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MechanicalRoutingSubsetBuilderSurroundingDataRecipeMethod Enumeration | Represents the method to use to determine the surrounding data corresponding to the routing design content that has been loaded. |
Property Detail¶
Fixtures¶
-
MechanicalRoutingSubsetBuilder.
Fixtures
¶ Returns or sets an option for inclusion of fixtures DE’s in the Routing Work.
-------------------------------------
Getter Method
Signature
Fixtures()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
Fixtures(includeFixtures)
Parameters: includeFixtures (bool) – New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Insulation¶
-
MechanicalRoutingSubsetBuilder.
Insulation
¶ Returns or sets an option for inclusion of insulation DE’s in the Routing Work Subset.
-------------------------------------
Getter Method
Signature
Insulation()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
Insulation(includeInsulation)
Parameters: includeInsulation (bool) – New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SurroundingDataProximityDistance¶
-
MechanicalRoutingSubsetBuilder.
SurroundingDataProximityDistance
¶ Returns or sets a proximity to Routing Content method has been selected to determine the surrounding content then this is the distance value used to perform the evaluation.
The units are in meters
-------------------------------------
Getter Method
Signature
SurroundingDataProximityDistance()
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurroundingDataProximityDistance(surroundingDataProximityDistance)
Parameters: surroundingDataProximityDistance (float) – New in version NX11.0.0.
License requirements: None.
SurroundingDataRecipeMethodType¶
-
MechanicalRoutingSubsetBuilder.
SurroundingDataRecipeMethodType
¶ Returns or sets the routing recipes
Assemblies.MechanicalRoutingSubsetBuilder
-------------------------------------
Getter Method
Signature
SurroundingDataRecipeMethodType()
Returns: Return type: NXOpen.Assemblies.MechanicalRoutingSubsetBuilderSurroundingDataRecipeMethod
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurroundingDataRecipeMethodType(surroundingDataRecipeMethod)
Parameters: surroundingDataRecipeMethod ( NXOpen.Assemblies.MechanicalRoutingSubsetBuilderSurroundingDataRecipeMethod
) –New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Method Detail¶
AppendSearchResultElementToSelectedList¶
-
MechanicalRoutingSubsetBuilder.
AppendSearchResultElementToSelectedList
¶ Appends the Search Result Element corresponding to the given Run ID to the SelectedSearchResultElement list on
NXOpen.Assemblies.MechanicalRoutingSubsetBuilder
.Signature
AppendSearchResultElementToSelectedList(runID)
Parameters: runID (str) – New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
GetConfigurationContextBuilder¶
-
MechanicalRoutingSubsetBuilder.
GetConfigurationContextBuilder
¶ Returns the configuration context builder which will be used by user to set revision rule or effectivity and then user needs to use
NXOpen.Assemblies.FindInCollaborativeDesign
to search for runs using object type RunElement.This is the builder which will be returned whenever you are creating new subsets. This will be NULL in edit mode scenario.
Signature
GetConfigurationContextBuilder()
Returns: Return type: NXOpen.PDM.ConfigurationContextBuilder
New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
GetSearchSubsetBuilder¶
-
MechanicalRoutingSubsetBuilder.
GetSearchSubsetBuilder
¶ The subset builder which is used for searching runs, the user will have to use
NXOpen.Assemblies.FindInCollaborativeDesign
to search for runs using object type RunElement.Signature
GetSearchSubsetBuilder()
Returns: Return type: NXOpen.Assemblies.SubsetBuilder
New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
RemoveAllSearchResultElementsFromSelectedList¶
-
MechanicalRoutingSubsetBuilder.
RemoveAllSearchResultElementsFromSelectedList
¶ Removes all the Search Result Element from the SelectedSearchResultElement list on
NXOpen.Assemblies.MechanicalRoutingSubsetBuilder
.Signature
RemoveAllSearchResultElementsFromSelectedList()
New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
RemoveSearchResultElementFromSelectedList¶
-
MechanicalRoutingSubsetBuilder.
RemoveSearchResultElementFromSelectedList
¶ Removes the Search Result Element corresponding to the given Run ID from the SelectedSearchResultElement list on
NXOpen.Assemblies.MechanicalRoutingSubsetBuilder
.Signature
RemoveSearchResultElementFromSelectedList(runID)
Parameters: runID (str) – New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SetRoutingSubsetAsWorkPart¶
-
MechanicalRoutingSubsetBuilder.
SetRoutingSubsetAsWorkPart
¶ The builder may generate multiple subsets.
This API will set the Routing Design Subset as the work part.
Signature
SetRoutingSubsetAsWorkPart()
New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SetSearchSubsetBuilder¶
-
MechanicalRoutingSubsetBuilder.
SetSearchSubsetBuilder
¶ Sets the subset builder which needs to be set by user to search runs, the user will have to use
NXOpen.Assemblies.FindInCollaborativeDesign
to search for runs using object type RunElement.Signature
SetSearchSubsetBuilder(subsetBuilder)
Parameters: subsetBuilder ( NXOpen.Assemblies.SubsetBuilder
) –New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
UpdateSubsetUsingConfigurationContext¶
-
MechanicalRoutingSubsetBuilder.
UpdateSubsetUsingConfigurationContext
¶ The routing subsets will be updated (e.
g. revision rule, effectivity) using the information available on the ConfigurationContext if the input is NULL. In case of valid input the corresponding subset will be updated with the information available on the ConfigurationContext.
Signature
UpdateSubsetUsingConfigurationContext(inputSubsetBuilder)
Parameters: inputSubsetBuilder ( NXOpen.Assemblies.SubsetBuilder
) –Returns: Return type: NXOpen.Assemblies.SubsetBuilder
New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Validate¶
-
MechanicalRoutingSubsetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.