Subset Class¶
-
class
NXOpen.Assemblies.
Subset
¶ Bases:
NXOpen.NXObject
A subset is a set of design elements within a collaborative design.
To create or edit an instance of this class, use
NXOpen.Assemblies.SubsetBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ComponentInWorkset | Returns the NXOpen.Assemblies.Component that corresponds to this subset in the workset NXOpen.Assemblies.ComponentAssembly . |
Description | Returns the description of this subset. |
DisplayExcludedDesignElements | Returns or sets the design elements excluded from spatial search to be displayed or not |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PartitionViewStyle | Returns or sets the partition view style to show. |
Prototype | Returns the prototype of this object if it is an occurrence. |
ShowSubsetStructure | Returns or sets the subset structure to be shown or not. |
SubsetType | Returns the type of plm object used to create subset. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddAllChildrenToSubset | Adds all the child components of the selected Reuse Design Element to the owning subset. |
AddConnectedByElements | Add Elements to a subset that reference the existing Design Elements in it by a Connection relation. |
AddDesignElementsToSubset | Adds the specified :py:class:`NXOpen.PDM.ModelElementRevision`s as members of the subset. |
AddInterpartParents | Add sources of interpart relationships (wave links in the subset and Connected To relationships for design features) that are not in the specified subset to the subset recipe. |
AddNewChildrenToSubset | If the Reuse Design Elements in the subset contain any new components which were not added to the subset because its owning workset was not the displayed part at the time of creation, then add those new components to the subset now. |
CanReplaceContentDefinition | Checks if the NXOpen.ContentDefinition object on the Subset can be replaced with the specified NXOpen.ContentDefinition object. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteFromCollaborativeDesign | Deletes the design elements from the owning NXOpen.CollaborativeDesign . |
DeletePositioningTask | Deletes the NXOpen.Assemblies.PositioningTask from this subset. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAllPositioningTasks | Gets all NXOpen.Assemblies.PositioningTask that belong to this subset. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDesignElementRevisionMembers | The :py:class:`NXOpen.PDM.DesignElementRevision`s that are members of this subset. |
GetDesignElementRevisionParents | The NXOpen.PDM.DesignElementRevision`s that have been loaded because they contain a :py:class:`NXOpen.PDM.DesignSubordinateRevision that belongs to this subset. |
GetDesignSubordinateRevisionMembers | The :py:class:`NXOpen.PDM.DesignSubordinateRevision`s that are members of this subset. |
GetDesignSubordinateRevisionParents | The NXOpen.PDM.DesignSubordinateRevision`s that have been loaded because they contain a :py:class:`NXOpen.PDM.DesignSubordinateRevision that belongs to this subset. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
HideCollaborativeDesignPreview | Hides the preview for the Collaborative Design in the graphics window if it was already displayed. |
IsCollaborativeDesignPreviewDisplayed | Is the preview for the Collaborative Design being displayed in the Graphics window. |
Prints a representation of this object to the system log file. | |
RemoveDesignElements | Removes the design elements from this subset. |
ReplaceContentDefinition | Replace the NXOpen.ContentDefinition object on the Subset. |
ReplayRecipe | Replay this subset. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetContentDefinition | Set a new NXOpen.ContentDefinition object on the Subset. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
ShowCollaborativeDesignPreview | Displays the preview for the Collaborative Design in the graphics window. |
Enumerations¶
SubsetContentType Enumeration | Represents the content type for a subset. |
SubsetPartitionViewStyleType Enumeration | Represents the type of partition view style to show for a subset. |
Property Detail¶
ComponentInWorkset¶
-
Subset.
ComponentInWorkset
¶ Returns the
NXOpen.Assemblies.Component
that corresponds to this subset in the worksetNXOpen.Assemblies.ComponentAssembly
.-------------------------------------
Getter Method
Signature
ComponentInWorkset()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Description¶
-
Subset.
Description
¶ Returns the description of this subset.
-------------------------------------
Getter Method
Signature
Description()
Returns: Return type: str New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
DisplayExcludedDesignElements¶
-
Subset.
DisplayExcludedDesignElements
¶ Returns or sets the design elements excluded from spatial search to be displayed or not
-------------------------------------
Getter Method
Signature
DisplayExcludedDesignElements()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
DisplayExcludedDesignElements(displayExcluded)
Parameters: displayExcluded (bool) – New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
IsOccurrence¶
-
Subset.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Subset.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Subset.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Subset.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Subset.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PartitionViewStyle¶
-
Subset.
PartitionViewStyle
¶ Returns or sets the partition view style to show.
-------------------------------------
Getter Method
Signature
PartitionViewStyle()
Returns: Return type: NXOpen.Assemblies.SubsetPartitionViewStyleType
New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
PartitionViewStyle(partitionViewStyle)
Parameters: partitionViewStyle ( NXOpen.Assemblies.SubsetPartitionViewStyleType
) –New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Prototype¶
-
Subset.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ShowSubsetStructure¶
-
Subset.
ShowSubsetStructure
¶ Returns or sets the subset structure to be shown or not.
-------------------------------------
Getter Method
Signature
ShowSubsetStructure()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
ShowSubsetStructure(showSubsetStructure)
Parameters: showSubsetStructure (bool) – New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SubsetType¶
-
Subset.
SubsetType
¶ Returns the type of plm object used to create subset.
-------------------------------------
Getter Method
Signature
SubsetType()
Returns: Return type: NXOpen.Assemblies.SubsetContentType
New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Method Detail¶
AddAllChildrenToSubset¶
-
Subset.
AddAllChildrenToSubset
¶ Adds all the child components of the selected Reuse Design Element to the owning subset.
Signature
AddAllChildrenToSubset(reuseDesignElements)
Parameters: reuseDesignElements (list of NXOpen.Assemblies.Component
) –New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
AddConnectedByElements¶
-
Subset.
AddConnectedByElements
¶ Add Elements to a subset that reference the existing Design Elements in it by a Connection relation.
A typical example will be to add Weld Design Features that reference any of the Design Elements in this subset. The recipe will be modified and explicit include terms will be added for each Element. The modified recipe will be replayed at the end of the operation. See
NXOpen.Assemblies.Subset.AddInterpartParents()
“Signature
AddConnectedByElements()
New in version NX8.5.1.
License requirements: nx_4gd_integration (“4th Generation Design”)
AddDesignElementsToSubset¶
-
Subset.
AddDesignElementsToSubset
¶ Adds the specified :py:class:`NXOpen.PDM.ModelElementRevision`s as members of the subset.
The subset recipe will be edited to include these elements with explicit include terms. A replay of the entire recipe will not be performed. The specified elements will be appended to the subset. See
NXOpen.Assemblies.Subset.ReplayRecipe()
Signature
AddDesignElementsToSubset(designElements)
Parameters: designElements (list of NXOpen.PDM.ModelElementRevision
) –Returns: Return type: NXOpen.PartLoadStatus
New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
AddInterpartParents¶
-
Subset.
AddInterpartParents
¶ Add sources of interpart relationships (wave links in the subset and Connected To relationships for design features) that are not in the specified subset to the subset recipe.
The recipe will be modified and explicit include terms will be added for each parent. The modified recipe will be replayed at the end of the operation.
Signature
AddInterpartParents()
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
AddNewChildrenToSubset¶
-
Subset.
AddNewChildrenToSubset
¶ If the Reuse Design Elements in the subset contain any new components which were not added to the subset because its owning workset was not the displayed part at the time of creation, then add those new components to the subset now.
Signature
AddNewChildrenToSubset()
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
CanReplaceContentDefinition¶
-
Subset.
CanReplaceContentDefinition
¶ Checks if the
NXOpen.ContentDefinition
object on the Subset can be replaced with the specifiedNXOpen.ContentDefinition
object.Signature
CanReplaceContentDefinition(contentDefinition)
Parameters: contentDefinition ( NXOpen.ContentDefinition
) –Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
DeleteFromCollaborativeDesign¶
-
Subset.
DeleteFromCollaborativeDesign
¶ Deletes the design elements from the owning
NXOpen.CollaborativeDesign
.Signature
DeleteFromCollaborativeDesign(designElement)
Parameters: designElement (list of NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
DeletePositioningTask¶
-
Subset.
DeletePositioningTask
¶ Deletes the
NXOpen.Assemblies.PositioningTask
from this subset.Signature
DeletePositioningTask(positioningTask)
Parameters: positioningTask ( NXOpen.Assemblies.PositioningTask
) –New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
FindObject¶
-
Subset.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAllPositioningTasks¶
-
Subset.
GetAllPositioningTasks
¶ Gets all
NXOpen.Assemblies.PositioningTask
that belong to this subset.Signature
GetAllPositioningTasks()
Returns: Return type: list of NXOpen.Assemblies.PositioningTask
New in version NX10.0.0.
License requirements: None.
GetDesignElementRevisionMembers¶
-
Subset.
GetDesignElementRevisionMembers
¶ The :py:class:`NXOpen.PDM.DesignElementRevision`s that are members of this subset.
Note that this does not include elements that have been loaded only because they contain a
NXOpen.PDM.DesignSubordinateRevision
that belongs to this subset. SeeGetDesignElementRevisionParents()
Signature
GetDesignElementRevisionMembers()
Returns: Return type: list of NXOpen.PDM.DesignElementRevision
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
GetDesignElementRevisionParents¶
-
Subset.
GetDesignElementRevisionParents
¶ The
NXOpen.PDM.DesignElementRevision`s that have been loaded because they contain a :py:class:`NXOpen.PDM.DesignSubordinateRevision
that belongs to this subset.Signature
GetDesignElementRevisionParents()
Returns: Return type: list of NXOpen.PDM.DesignElementRevision
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
GetDesignSubordinateRevisionMembers¶
-
Subset.
GetDesignSubordinateRevisionMembers
¶ The :py:class:`NXOpen.PDM.DesignSubordinateRevision`s that are members of this subset.
Note that this does not include elements that have been loaded only because they contain a
NXOpen.PDM.DesignSubordinateRevision
that belongs to this subset. SeeGetDesignSubordinateRevisionParents()
Signature
GetDesignSubordinateRevisionMembers()
Returns: Return type: list of NXOpen.PDM.DesignSubordinateRevision
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
GetDesignSubordinateRevisionParents¶
-
Subset.
GetDesignSubordinateRevisionParents
¶ The
NXOpen.PDM.DesignSubordinateRevision`s that have been loaded because they contain a :py:class:`NXOpen.PDM.DesignSubordinateRevision
that belongs to this subset.Signature
GetDesignSubordinateRevisionParents()
Returns: Return type: list of NXOpen.PDM.DesignSubordinateRevision
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
HideCollaborativeDesignPreview¶
-
Subset.
HideCollaborativeDesignPreview
¶ Hides the preview for the Collaborative Design in the graphics window if it was already displayed.
See
ShowCollaborativeDesignPreview()
.Signature
HideCollaborativeDesignPreview()
New in version NX8.5.1.
License requirements: nx_4gd_integration (“4th Generation Design”)
IsCollaborativeDesignPreviewDisplayed¶
-
Subset.
IsCollaborativeDesignPreviewDisplayed
¶ Is the preview for the Collaborative Design being displayed in the Graphics window.
Signature
IsCollaborativeDesignPreviewDisplayed()
Returns: Return type: bool New in version NX8.5.1.
License requirements: nx_4gd_integration (“4th Generation Design”)
Print¶
-
Subset.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveDesignElements¶
-
Subset.
RemoveDesignElements
¶ Removes the design elements from this subset.
This will not delete the design element from the owning
NXOpen.CollaborativeDesign
.Signature
RemoveDesignElements(designElements)
Parameters: designElements (list of NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
ReplaceContentDefinition¶
-
Subset.
ReplaceContentDefinition
¶ Replace the
NXOpen.ContentDefinition
object on the Subset.Signature
ReplaceContentDefinition(contentDefinition)
Parameters: contentDefinition ( NXOpen.ContentDefinition
) –New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
ReplayRecipe¶
-
Subset.
ReplayRecipe
¶ Replay this subset.
This will perform a search using the current subset recipe and configuration. The contents of the subset will be changed accordingly.
Signature
ReplayRecipe()
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SetContentDefinition¶
-
Subset.
SetContentDefinition
¶ Set a new
NXOpen.ContentDefinition
object on the Subset.Signature
SetContentDefinition(contentDefinition)
Parameters: contentDefinition ( NXOpen.ContentDefinition
) –New in version NX11.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SetName¶
-
Subset.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
ShowCollaborativeDesignPreview¶
-
Subset.
ShowCollaborativeDesignPreview
¶ Displays the preview for the Collaborative Design in the graphics window.
The preview is stored as a JT dataset on the Collaborative Design. Any transformation specific to this subset will also be applied to the preview. isPreviewAvailable will be false if no JT dataset could be found. See
HideCollaborativeDesignPreview()
.Signature
ShowCollaborativeDesignPreview()
Returns: Return type: bool New in version NX8.5.1.
License requirements: nx_4gd_integration (“4th Generation Design”)