ReplaceComponentBuilderComponentReferenceSet Enumeration¶
NXOpen.Assemblies.ReplaceComponentBuilder.ComponentReferenceSet is an alias for NXOpen.Assemblies.ReplaceComponentBuilderComponentReferenceSet
-
class
NXOpen.Assemblies.
ReplaceComponentBuilderComponentReferenceSet
¶ Bases:
object
Represents possible reference set for replacement part
Enum Members
Enum Member Enum Member Description Maintain Maintain the reference set of the component being replaced outEntirePart Set the reference set to Entire PartEmpty Set the reference to EmptyOthers Set the specified reference set-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-