ConstraintDisplayBuilderVisibleConstraintsRuleOptions Enumeration¶
NXOpen.Assemblies.ConstraintDisplayBuilder.VisibleConstraintsRuleOptions is an alias for NXOpen.Assemblies.ConstraintDisplayBuilderVisibleConstraintsRuleOptions
-
class
NXOpen.Assemblies.
ConstraintDisplayBuilderVisibleConstraintsRuleOptions
¶ Bases:
object
This enum is used to control which constraints are treated as connected to the selected components.
Enum Members
Enum Member Enum Member Description BetweenComponents Show only constraints that refer only to selected componentsConnectedToComponents Show only constraints that refer at least once to a selected component-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-