LoadInterpartDataBuilder Class¶
-
class
NXOpen.Assemblies.
LoadInterpartDataBuilder
¶ Bases:
NXOpen.Builder
Represents a builder:py:class:NXOpen.Assemblies.LoadInterpartDataBuilder
To create a new instance of this class, use
NXOpen.Assemblies.AssemblyManager.CreateLoadInterpartDataBuilder()
Default values.
Property Value OpenUnloadedParents None SelectionScope AllPartsInDisplayedAssembly New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
OpenUnloadedParents | Returns or sets the open unloaded parents level type |
SelectionScope | Returns or sets the selection scope type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFailedParts | Returns an array of the parts that failed to load and update @return Array of the part tags failed to load and update |
GetLoadInterpartDataStatus | Returns part load status and delayed update status for the part which failed to load and update |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LoadInterpartDataBuilderOpenUnloadedParentsType Enumeration | Represents the load interpart parent level types |
LoadInterpartDataBuilderSelectionScopeType Enumeration | Represents the load interpart selection scope types |
Property Detail¶
OpenUnloadedParents¶
-
LoadInterpartDataBuilder.
OpenUnloadedParents
¶ Returns or sets the open unloaded parents level type
-------------------------------------
Getter Method
Signature
OpenUnloadedParents()
Returns: Return type: NXOpen.Assemblies.LoadInterpartDataBuilderOpenUnloadedParentsType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OpenUnloadedParents(openUnloadedParents)
Parameters: openUnloadedParents ( NXOpen.Assemblies.LoadInterpartDataBuilderOpenUnloadedParentsType
) –New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
SelectionScope¶
-
LoadInterpartDataBuilder.
SelectionScope
¶ Returns or sets the selection scope type
-------------------------------------
Getter Method
Signature
SelectionScope()
Returns: Return type: NXOpen.Assemblies.LoadInterpartDataBuilderSelectionScopeType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionScope(selectionScope)
Parameters: selectionScope ( NXOpen.Assemblies.LoadInterpartDataBuilderSelectionScopeType
) –New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
Method Detail¶
GetFailedParts¶
-
LoadInterpartDataBuilder.
GetFailedParts
¶ Returns an array of the parts that failed to load and update
Signature
GetFailedParts()
Returns: Array of the part tags failed to load and update :rtype: list of
NXOpen.BasePart
New in version NX6.0.0.
License requirements: None.
GetLoadInterpartDataStatus¶
-
LoadInterpartDataBuilder.
GetLoadInterpartDataStatus
¶ Returns part load status and delayed update status for the part which failed to load and update
Signature
GetLoadInterpartDataStatus(part)
Parameters: part ( NXOpen.BasePart
) – Failed part tagReturns: a tuple Return type: A tuple consisting of (loadStatus, delayedUpdateStatus). loadStatus is a NXOpen.PartLoadStatus
. Part load status for the failed partdelayedUpdateStatus is aNXOpen.PartDelayedUpdateStatus
. Delayed update status data status for the failed partNew in version NX6.0.0.
License requirements: None.
Validate¶
-
LoadInterpartDataBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.