ClearanceSetReanalyzePairCalculationMethod Enumeration¶
NXOpen.Assemblies.ClearanceSet.ReanalyzePairCalculationMethod is an alias for NXOpen.Assemblies.ClearanceSetReanalyzePairCalculationMethod
-
class
NXOpen.Assemblies.
ClearanceSetReanalyzePairCalculationMethod
¶ Bases:
object
The analysis method to use when reanalyzing a pair.
Enum Members
Enum Member Enum Member Description UseStoredMethod Use the clearance set’s defined analysis method.Lightweight ExactIfLoaded Exact -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-